8.7.8.43. GEL_LoadBin()ΒΆ
Loads a binary file.
Syntax
GEL_LoadBin( "file_path", [start_address], ["cpu_name"], ["board_name"] );
Parameters
file_path: Path to the binary file to be loaded. The file_path must be enclosed in quotation marks.
start_address (optional): Address on the target at which the contents of the file should be written. Default is 0.
cpu_name (optional): Names the CPU on which to load the file (useful in a multiprocessor environment). The cpuName must be enclosed in quotation marks.
board_name (optional): is the text string specified as the Board Name in the target configuration. The boardName must be enclosed in quotation marks.
Description
Loads a raw binary file into target memory, starting at the specified address. The entire contents of the file are treated as binary data to be written to the target memory.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: No
Example
GEL_LoadBin( "C:/path/to/file.bin", 0x8000 );
GEL_LoadBin( "C:/path/to/file.bin", 0x8000, "cpu_a", "Emulator" );
Related Topics