8.7.8.39. GEL_IsInRealtimeModeΒΆ

Called every time a target is connected. GEL built-in function that can be called at any time to determine if the target is in realtime mode.

Syntax

GEL_IsInRealtimeMode();

Description

The function returns 0 is the DSP is currently in Stop mode and 1 if it is in Real Time Mode. Some targets cannot enter Real Time mode; for those cases, the function will always return 0. (See real-time mode)

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Example

OnTargetConnect()
{
    if( GEL_IsInRealtimeMode() )
    {
        // The target was connected in realtime mode
    }
    else
    {
        //The target was connected in stop mode
    }
}

Related Topics

GEL_DisableRealtime

GEL_EnableRealtime