8.7.8.53. GEL_MatchesConnection()ΒΆ
Queries if the connection name matches the specified regular expression.
Syntax
GEL_MatchesConnection( "regex" );
Parameters
regex: Regular expression to match against the connection name. The regular expression must be enclosed in quotation marks.
Description
Returns 1 if the provided regular expression matches the connection of the current GEL context's target. Returns 0 otherwise. The connection name is the connectionType in the connection's xml definition file.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
GEL_MatchesConnection("JLINK");
GEL_MatchesConnection("TIXDS.*");