8.7.8.7. GEL_BreakPtDel()ΒΆ

Delete a breakpoint.

Syntax

GEL_BreakPtDel( address );

Parameters

address: identifies the location of the breakpoint.

Description

This function clears a software breakpoint at a specific address. If there is no software breakpoint set at address, nothing happens. The address can be an absolute address, any C expression, the name of a C function, or the name of an assembly language label.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: No

Example

GEL_BreakPtDel(0x2000);
GEL_BreakPtDel(TargetLabel + 100);

Related Topics

GEL_BreakPtAdd

GEL_BreakPtReset