8.7.8.15. GEL_DisconnectΒΆ
GEL built-in function that can be called on a connected target to disconnect it.
Syntax
GEL_Disconnect();
Description
The function disconnects the target and then returns. It throws an exception if the target is already disconnected or cannot be disconnected.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Related Topics