7.7.8.127. OnRestart()ΒΆ

GEL callback function called when the program is restarted.

Syntax

OnRestart( intnErrorCode );

Parameters

nErrorCode: 0 (zero) indicates success.

Description

If defined in a loaded GEL file, OnRestart() is called when the program is restarted.

Example

OnRestart(int nErrorCode)
{
    if (nErrorCode)
    {
        GEL_TextOut("An error occurred while restarting. -%d-\n",,,,, nErrorCode);
    }
    else
    {
        GEL_TextOut("Restart was successful. -%d-\n",,,,, nErrorCode);
    }
}