7.7.8.45. GEL_LoadProgramOnly()ΒΆ
Loads a program without loading symbol information
Syntax
GEL_LoadProgramOnly( "file_path", ["cpuName"], ["boardName"], [is_data_only] );
Parameters
file_path: The path to the file to be loaded. The file_path must be enclosed in quotation marks.
cpuName (optional): Names the CPU on which to load the file (useful in a multiprocessor environment). The cpuName must be enclosed in quotation marks.
boardName (optional): is the text string specified as the Board Name in the target configuration. The boardName must be enclosed in quotation marks.
is_data_only (optional): If non-zero, indicates that we should just load the contents of the file and not perform other debugger events related to loading a program. For example, the debugger will not set the PC or call the GEL callbacks related to program loads. Default is 0 (false).
Description
Like GEL_Load <GEL_Load.html>, this function downloads both program code and data onto the target at the addresses specified in the file. However, no attempt will be made by the debugger to load symbol information.
Supported file formats
- COFF - ELF - S-Record - Intel Hex - Tektronix Hex - TI HEX (also known
as TI-txt)
If the file is not in the current directory, provide a full path name within the string. A double backslash escape sequence is required to ensure that you get a backslash into the fileName.
The cpuName must match the CPU name as configured in the multiprocessor setup. In a single processor system, you do not need to fill this field.
Synchronous
Synchronous from GEL: No
Completely synchronous: No
Example
GEL_LoadProgramOnly("c:\\mydir\\myfile.out", "cpu_a", "Emulator");
Related Topics