7.7.8.67. GEL_ReConnectΒΆ
GEL built-in function that can be called on a connected target to re-send the connection sequence to it.
Syntax
GEL_ReConnect();
Description
The function effectively disconnects and connects the target and then returns. Unlike calling GEL_Disconnect() followed by GEL_Connect(), it will not generate any GEL callbacks nor trigger a UI update. This function exists only for specific devices that require the jtag/swd connection sequence to be re-sent in specific scenarios, such as when communicating with a bootloader.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Related Topics