7.7.8.34. GEL_HWBreakPtDel()ΒΆ

Removes a hardware breakpoint.

Syntax

GEL_HWBreakPtDel( address );

Parameters

address: is the memory location of the hardware breakpoint to be removed.

Description

This function removes any hardware breakpoint currently set at the specified address, if the target supports it.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: No

Related Topics

GEL_HWBreakPtAdd

GEL_HWBreakPtReset