7.7.8.22. GEL_GetBoolDriverPropertyΒΆ

Return the value of a boolean driver property

Syntax

GEL_GetBoolDriverProperty( propertyName );

Parameters

propertyName: specifies the property name

Description

Return the value of the property

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Example

int hasBoardReset = GEL_GetBoolDriverProperty("Use Board Reset");
string deviceId = GEL_GetStringDriverProperty("device.identify");
int traceId = GEL_GetNumericDriverProperty("device.traceId");

Related Topics

GEL_GetBoolDebugProperty

GEL_GetNumericDebugProperty

GEL_GetStringDebugProperty

GEL_GetNumericDriverProperty

GEL_GetStringDriverProperty

GEL_GetBoolTargetDbProperty

GEL_GetNumericTargetDbProperty

GEL_GetStringTargetDbProperty