7.7.8.29. GEL_GetStringTargetDbPropertyΒΆ
Return the value of a string driver/device property
Syntax
GEL_GetStringTargetDbProperty( propertyName );
Parameters
propertyName: specifies the property name
Description
Return the value of the property
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
int bHaltOnConnect = GEL_GetBoolTargetDbProperty("haltOnConnectByDefault");
string defConn = GEL_GetStringTargetDbProperty("DefaultConnection");
int numIntrs = GEL_GetNumericTargetDbProperty("Number of Interrupt Supported");
Related Topics