7.7.8.11. GEL_ConnectΒΆ
GEL built-in function that can be called on a disconnected target to connect it.
Syntax
GEL_Connect();
Description
The function connects the target and then returns. It throws an exception if the target is already connected or fails to connect.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Related Topics