7.7.2. Built-in GEL Functions¶
There are several built-in GEL functions that allow you to control the state of the actual/simulated target, access the actual/simulated target memory locations, and to display results in the output window.
All GEL built-in functions are preceded with the prefix GEL_ to ensure they are not confused with user-defined GEL functions. If you wish to avoid preceding all calls to GEL built-in functions with GEL_ you can define functions with your own names and call the GEL built-in functions within your functions. For example, the following GEL function allows you to call the GEL_Load() built-in functions just by typing-in Load.
Load(a)
{
GEL_Load(a);
}
All built-in GEL functions and user-defined GEL functions consisting of GEL statements can be invoked directly from the Debug Console View. To invoke any GEL statement or user-defined function, enter the appropriate function call in the console and press the Enter key to evaluate the expression. In this example, the built-in GEL function GEL_Go() is called.