7.9.8.110. OnReset()¶
GEL callback function called after the target processor has been reset.
Syntax
OnReset( int nErrorCode );
Parameters
nErrorCode 0 (zero) indicates success.
Description
If defined in a loaded GEL file, OnReset() is called after the target processor has been reset.
Example
OnReset(int nErrorCode)
{
if (nErrorCode)
GEL_TextOut("An error occurred while resetting. -%d-n",,,,,
nErrorCode);
else
GEL_TextOut("Reset was successful. -%d-n",,,,, nErrorCode);
}