7.9.8.36. GEL_IsInRealtimeMode

Called every time a target is connected. GEL built-in function that can be called at any time to determine if the target is in realtime mode.

Syntax

GEL_IsInRealtimeMode()

Parameters

None

Description

The function returns 0 is the DSP is currently in Stop mode and 1 if it is in Real Time Mode. Some targets cannot enter Real Time mode; for those cases, the function will always return 0. (See real-time mode)

Synchronous

Synchronous from GEL: Yes

Completely synchronous: Yes

Example

OnTargetConnect()

{ if( GEL_IsInRealtimeMode() )

{

// The target was connected in realtime mode

}

else

{

//The target was connected in stop mode

}

Related Topics