7.9.8.16. GEL_EnableClock()¶
Enables or disables the profile clock.
Syntax
GEL_EnableClock([bool enable]);
Parameters
[optional]
0 disables the clock.
1 enables the clock
blank enables the clock
Description
This function is used to enable or disable the profile clock.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
GEL_EnableClock(); //Enable Clock
GEL_EnableClock(0); //Disable Clock
GEL_EnableClock(1); //Enable Clock