7.9.8.49. GEL_MemoryLoadData()¶
Loads a block of memory from a file.
Syntax
GEL_MemoryLoadData(startAddress, page, length, "fileName" )
Parameters
startAddress is the first address in the block.
page identifies the type of memory to fill: 0 (Program memory), 1 (Data memory) or 2 (I/O space)
For processors that do not have more than one type of memory, use 0 for this Parameters. For simulated targets, the I/O space Parameters is not supported.
length defines the number of values to load from the file
fileName name of the file to load data from. The fileName must be enclosed in quotation marks.
Description
GEL_MemoryLoadData() is an extention to GEL_MemoryLoad() and supports loading data in addtional formats to target memory from a specified file.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
GEL_MemoryLoadData( 0x100, 0 , 0x100, "c:\mydir\myfile.dat" );
Related Topics