7.9.8.93. GEL_SyncRun

Performs a run operation on every target that is in the same group as the current target.

Format

GEL_SyncRun( );

Parameters

None.

Description

Performs a run operation on every target that is in the same group as the current target. The operation performed is the same as the run command that may be invoked from the PDM debug menu.

As with the other synchronous operations, the operation is performed on all targets simultaneously.

Synchronous

Synchronous from GEL: No

Completely synchronous: No

Example

GEL_SyncRun( );

Related Topics

GEL_SyncHalt

GEL_SyncStepInto

GEL_SyncStepOut

GEL_SyncStepOver