7.9.8.97. GEL_System()

Executes a DOS command.

Syntax

GEL_System("dosCommand" [, param1, param2, .. param4] );

Parameters

dosCommand: specifies the DOS command (which may contain optional format specifiers) that is to be executed.

param1..param4(optional) name additional parameters that are substituted in the dosCommand when a format specifier is encountered. These parameters allow you to pass values to the DOS command.

Description

The GEL_System function allows you to execute DOS commands from within the IDE. The output of the DOS command is sent to an output window within the IDE. The DOS command can only be one that produces a text output and does not require additional user input once it starts executing.

The DOS command that is executed is actually the formatted string given by dosCommand and the additional parameters (parm1..parm4). This allows you to pass additional parameters (including values that are defined on the target) to the DOS command.

Format specifications always begin with a percent sign (%) and are read left to right. When the first format specification (if any) is encountered, the value of the first argument after format is converted and printed in dosCommand. The second format specification causes the second argument to be converted and printed, and so on. If there are more arguments than there are format specifications, the extra arguments are ignored.

The GEL_System() GEL function is implemented using proprietary technology and can be used to extend the capabilities of the IDE. You can use it to perform tasks (such as compiling) in the background and pipe the results to the output window within the IDE.

Synchronous

Synchronous from GEL: No

Completely synchronous: No

Example

GEL_System("dir");
GEL_System("dir *.dat")

Which is equivalent to:

GEL_System("dir %s", "*.dat");

But not GEL_System("dir", "*.dat");

GEL_System("myfunc %f %d %s", targVar, 3, "-ol");

If we assume that targVar is a variable defined on the target and that its value is 3.14, then the final DOS command that is executed is: >>myfunc 3.14 3 -ol