7.9.8.96. GEL_SyncStepOver¶
Performs a StepOver operation on every target that is in the same group as the current target.
Format
GEL_SyncStepOver([iterations]);
Parameters
iterations(optional) specifies the number of times the command is to be repeated. If iterations is not specified, a single StepOver is performed.
Description
Performs a StepOver operation on every target that is in the same group as the current target. The operation performed is the same as the StepOver option selected from the PDM debug menu.
As with the other synchronous operations, the operation is performed on all targets simultaneously.
Synchronous
Synchronous from GEL: No
Completely synchronous: No
Example
GEL_SyncStepOver(5);
GEL_SyncStepOver ( );
Related Topics