7.9.8.27. GEL_Go()¶
Runs to specified address.
Syntax
GEL_Go( [address] );
Parameters
address(optional) is the stop address.
Description
The GEL_Go function executes code up to a specific point in the program. The address Parameters is treated as a program-memory address. If you do not supply an address, then GEL_Go becomes equivalent to the GEL_Run GEL function.
Synchronous
Synchronous from GEL: Yes, only if location is given
Completely synchronous: Yes, only if location is given
Example
GEL_Go();
GEL_Go(main);
Related Topics