7.9.8.54. GEL_PinConnect()¶
For simulator only, connects a data file to an external interrupt pin.
Syntax
GEL_PinConnect( "pinName", "fileName" );
Parameters
pinName names the external interrupt pin. The pinName must be enclosed in quotation marks.
fileNamenames the data file that specifies interrupt intervals. The fileName must be enclosed in quotation marks.
Description
The simulator allows you to simulate external interrupt signals. This function connects a data file that specifies interrupt intervals to the specified external interrupt pin.
If the file is not in the current directory, provide a full path name within the string. A double backslash escape sequence is required to ensure that you get a backslash into the fileName Parameters.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
GEL_PinConnect("INT0", "c:\mydir\myfile.dat");
Related Topics