7.9.8.58. GEL_ProbePtAdd()¶
Adds a software breakpoint at the specified address.
Syntax
GEL_ProbePtAdd(address);
Parameters
addressspecifies the location of the breakpoint. If address is a string Parameters, a symbolic breakpoint will be set at that location and re-evaluated whenever symbols change. Otherwise, a breakpoint will be set at the specified address.
Description
This function sets a software breakpoint at a specified address. The address can be any GEL expression that evaluates to a program address, or a string that specifies a symbolic location. The breakpoint must be manually connected to a window or a file I/O operation before it will do anything.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: No
Example
GEL_ProbePtAdd(PC + 100);
GEL_ProbePtAdd(0x2000);
GEL_ProbePtAdd("main");
Related Topics