7.9.8.32. GEL_HWBreakPtDisable

Disables a hardware breakpoint at the specified address.

Format

GEL_HWBreakPtDisable(address);

Parameters

address specifies the location of the hardware breakpoint.

Description

The hardware breakpoint at the specified address is disabled. If the breakpoint does not exist or is already disabled, no action is taken. This function does not disable software breakpoints.

Synchronous

Synchronous from GEL: Yes

Completely synchronous: No

Example

GEL_HWBreakPtDisable(0x2000);

GEL_HWBreakPtDisable(main + 100);

Related Topics

GEL_HWBreakPtAdd()

GEL_HWBreakPtDel()

GEL_HWBreakPtReset()

GEL_BreakPtDisable