7.9.8.71. GEL_RunF()

Runs free.

Syntax

GEL_RunF();

Parameters

None.

Description

This function disables breakpoints before it starts executing code on the target. It also disconnects from the target system. This is useful if you need to perform a hardware reset on your target system or if you need to disconnect the JTAG or MPSD cable. The Code Composer Studio debugger reconnects to the target system and enables breakpoints if any access is requested on the target system (e.g., memory read), or if the user halts the processor.

Synchronous

Synchronous from GEL: No

Completely synchronous: No

Example

GEL_RunF();

Related Topics

GEL_Restart

GEL_Go

GEL_Halt

GEL_Run