7.9.8.92. GEL_SyncHalt

Perform a halt operation on every target that is in the same group as the current target.

Format

GEL_SyncHalt( );

Parameters

None

Description

Performs a halt operation on every target that is in the same group as the current target. The operation performed is the same as the halt command that may be invoked from the PDM debug menu.

As with the other synchronous operations, the operation is performed on all targets simultaneously.

Synchronous

Synchronous from GEL: No

Completely synchronous: No

Example

GEL_SyncHalt( );

Related Topics

GEL_SyncRun

GEL_SyncStepInto

GEL_SyncStepOut

GEL_SyncStepOver