7.7.8.44. GEL_LoadGel()¶
Loads a GEL file.
Syntax
GEL_LoadGel( "fileName" );
Parameters
fileName: names the GEL file to be loaded. The fileName must be enclosed in quotation marks.
Description
This function loads the specified GEL file.
If the file is not in the current directory, provide a full path name within the string. A double backslash escape sequence is required to ensure that you get a backslash into the fileName Parameters.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
GEL_LoadGel("c:\\mydir\\myfile.gel");
Related Topics