CADC12_B_configureMemoryParam | Used in the ADC12_B_configureMemory() function as the param parameter |
CADC12_B_initParam | Used in the ADC12_B_init() function as the param parameter |
CCalendar | Used in the RTC_B_initCalendar() function as the CalendarTime parameter |
CComp_E_initParam | Used in the Comp_E_init() function as the param parameter |
CDMA_initParam | Used in the DMA_init() function as the param parameter |
CESI_AFE1_InitParams | |
CESI_AFE2_InitParams | |
CESI_PSM_InitParams | |
CESI_TSM_InitParams | |
CESI_TSM_StateParams | |
CEUSCI_A_SPI_changeMasterClockParam | Used in the EUSCI_A_SPI_changeMasterClock() function as the param parameter |
CEUSCI_A_SPI_initMasterParam | Used in the EUSCI_A_SPI_initMaster() function as the param parameter |
CEUSCI_A_SPI_initSlaveParam | Used in the EUSCI_A_SPI_initSlave() function as the param parameter |
CEUSCI_A_UART_initParam | Used in the EUSCI_A_UART_init() function as the param parameter |
CEUSCI_B_I2C_initMasterParam | Used in the EUSCI_B_I2C_initMaster() function as the param parameter |
CEUSCI_B_I2C_initSlaveParam | Used in the EUSCI_B_I2C_initSlave() function as the param parameter |
CEUSCI_B_SPI_changeMasterClockParam | Used in the EUSCI_B_SPI_changeMasterClock() function as the param parameter |
CEUSCI_B_SPI_initMasterParam | Used in the EUSCI_B_SPI_initMaster() function as the param parameter |
CEUSCI_B_SPI_initSlaveParam | Used in the EUSCI_B_SPI_initSlave() function as the param parameter |
CLCD_C_initParam | Used in the LCD_C_init() function as the initParams parameter |
CLEA_addLongMatrixParams | Parameter structure that should be paired with the LEA_addLongMatrix command when using LEA_invokeCommand() |
CLEA_addMatrixParams | Parameter structure that should be paired with the LEA_addMatrix command when using LEA_invokeCommand() |
CLEA_biquadWithBiasAndMinMaxParams | Parameter structure that should be paired with the LEA_biquadWithBiasAndMinMax command when using LEA_invokeCommand() |
CLEA_bitReverseComplexEvenParams | Parameter structure that should be paired with the LEA_bitReverseComplexEven command when using LEA_invokeCommand() |
CLEA_bitReverseComplexLongEvenParams | Parameter structure that should be paired with the LEA_bitReverseComplexLongEven command when using LEA_invokeCommand() |
CLEA_bitReverseComplexLongOddParams | Parameter structure that should be paired with the LEA_bitReverseComplexLongOdd command when using LEA_invokeCommand() |
CLEA_bitReverseComplexOddParams | Parameter structure that should be paired with the LEA_bitReverseComplexOdd command when using LEA_invokeCommand() |
CLEA_deinterleaveEvenEvenParams | Parameter structure that should be paired with the LEA_deinterleaveEvenEven command command when using LEA_invokeCommand() |
CLEA_deinterleaveEvenOddParams | Parameter structure that should be paired with the LEA_deinterleaveEvenOdd command command when using LEA_invokeCommand() |
CLEA_deinterleaveLongParams | Parameter structure that should be paired with the LEA_deinterleaveLong command command when using LEA_invokeCommand() |
CLEA_deinterleaveOddEvenParams | Parameter structure that should be paired with the LEA_deinterleaveOddEven command command when using LEA_invokeCommand() |
CLEA_deinterleaveOddOddParams | Parameter structure that should be paired with the LEA_deinterleaveOddOdd command command when using LEA_invokeCommand() |
CLEA_fftComplexAutoScalingParams | Parameter structure that should be paired with the LEA_fftComplexAutoScaling command when using LEA_invokeCommand() |
CLEA_fftComplexFixedScalingParams | Parameter structure that should be paired with the LEA_fftComplexFixedScaling command when using LEA_invokeCommand() |
CLEA_fftComplexLongParams | Parameter structure that should be paired with the LEA_fftComplexLong command when using LEA_invokeCommand() |
CLEA_fftLongParams | Parameter structure that should be paired with the LEA_fftLong command when using LEA_invokeCommand() |
CLEA_fftParams | Parameter structure that should be paired with the LEA_fft command when using LEA_invokeCommand() |
CLEA_firComplexLongParams | Parameter structure that should be paired with the LEA_firComplexLong command when using LEA_invokeCommand() |
CLEA_firComplexParams | Parameter structure that should be paired with the LEA_firComplex command when using LEA_invokeCommand() |
CLEA_firLongParams | Parameter structure that should be paired with the LEA_firLong command when using LEA_invokeCommand() |
CLEA_firParams | Parameter structure that should be paired with the LEA_fir command when using LEA_invokeCommand() |
CLEA_goertzelParams | Parameter structure that should be paired with the LEA_goertzel command when using LEA_invokeCommand() |
CLEA_iirParams | Parameter structure that should be paired with the LEA_iir command when using LEA_invokeCommand() |
CLEA_macComplexConjugateMatrixParams | Parameter structure that should be paired with the LEA_macComplexConjugateMatrix command when using LEA_invokeCommand() |
CLEA_macComplexMatrixParams | Parameter structure that should be paired with the LEA_macComplexMatrix command when using LEA_invokeCommand() |
CLEA_macLongMatrixParams | Parameter structure that should be paired with the LEA_macLongMatrix command when using LEA_invokeCommand() |
CLEA_macMatrixParams | Parameter structure that should be paired with the LEA_macMatrix command when using LEA_invokeCommand() |
CLEA_macParams | Parameter structure that should be paired with the LEA_mac command when using LEA_invokeCommand() |
CLEA_maxLongMatrixParams | Parameter structure that should be paired with the LEA_maxLongMatrix command when using LEA_invokeCommand() |
CLEA_maxMatrixParams | Parameter structure that should be paired with the LEA_maxMatrix command when using LEA_invokeCommand() |
CLEA_maxParams | Parameter structure that should be paired with the LEA_max command when using LEA_invokeCommand() |
CLEA_maxUnsignedLongMatrixParams | Parameter structure that should be paired with the LEA_maxUnsignedLongMatrix command when using LEA_invokeCommand() |
CLEA_maxUnsignedMatrixParams | Parameter structure that should be paired with the LEA_maxUnsignedMatrix command when using LEA_invokeCommand() |
CLEA_maxUnsignedParams | Parameter structure that should be paired with the LEA_maxUnsigned command when using LEA_invokeCommand() |
CLEA_minLongMatrixParams | Parameter structure that should be paired with the LEA_minLongMatrix command when using LEA_invokeCommand() |
CLEA_minMatrixParams | Parameter structure that should be paired with the LEA_minMatrix command when using LEA_invokeCommand() |
CLEA_minParams | Parameter structure that should be paired with the LEA_mi command when using LEA_invokeCommand() |
CLEA_minUnsignedLongMatrixParams | Parameter structure that should be paired with the LEA_minUnsignedLongMatrix command when using LEA_invokeCommand() |
CLEA_minUnsignedMatrixParams | Parameter structure that should be paired with the LEA_minUnsignedMatrix command when using LEA_invokeCommand() |
CLEA_minUnsignedParams | Parameter structure that should be paired with the LEA_minUnsigned command when using LEA_invokeCommand() |
CLEA_moveLongListParams | Parameter structure that should be paired with the LEA_moveList command command when using LEA_invokeCommand() |
CLEA_mpyComplexMatrixParams | Parameter structure that should be paired with the LEA_mpyComplexMatrix command when using LEA_invokeCommand() |
CLEA_mpyLongMatrixParams | Parameter structure that should be paired with the LEA_mpyLongMatrix command when using LEA_invokeCommand() |
CLEA_mpyMatrixParams | Parameter structure that should be paired with the LEA_mpyMatrix command when using LEA_invokeCommand() |
CLEA_mpyMatrixRowParams | Parameter structure that should be paired with the LEA_mpyMatrixRow command when using LEA_invokeCommand() |
CLEA_polynomialLongParams | Parameter structure that should be paired with the LEA_polynomialLong command when using LEA_invokeCommand() |
CLEA_polynomialParams | Parameter structure that should be paired with the LEA_polynomial command when using LEA_invokeCommand() |
CLEA_polynomialScalarParams | Parameter structure that should be paired with the LEA_polynomialScalar command when using LEA_invokeCommand() |
CLEA_subLongMatrixParams | Parameter structure that should be paired with the LEA_subLongMatrix command when using LEA_invokeCommand() |
CLEA_subMatrixParams | Parameter structure that should be paired with the LEA_subMatrix command when using LEA_invokeCommand() |
CMPU_initThreeSegmentsParam | Used in the MPU_initThreeSegments() function as the param parameter |
CRTC_B_configureCalendarAlarmParam | Used in the RTC_B_configureCalendarAlarm() function as the param parameter |
CRTC_C_configureCalendarAlarmParam | Used in the RTC_C_configureCalendarAlarm() function as the param parameter |
Cs_Peripheral_Memory_Data | |
Cs_TLV_ADC_Cal_Data | |
Cs_TLV_Die_Record | |
Cs_TLV_REF_Cal_Data | |
Cs_TLV_Timer_D_Cal_Data | |
CTimer_A_initCaptureModeParam | Used in the Timer_A_initCaptureMode() function as the param parameter |
CTimer_A_initCompareModeParam | Used in the Timer_A_initCompareMode() function as the param parameter |
CTimer_A_initContinuousModeParam | Used in the Timer_A_initContinuousMode() function as the param parameter |
CTimer_A_initUpDownModeParam | Used in the Timer_A_initUpDownMode() function as the param parameter |
CTimer_A_initUpModeParam | Used in the Timer_A_initUpMode() function as the param parameter |
CTimer_A_outputPWMParam | Used in the Timer_A_outputPWM() function as the param parameter |
CTimer_B_initCaptureModeParam | Used in the Timer_B_initCaptureMode() function as the param parameter |
CTimer_B_initCompareModeParam | Used in the Timer_B_initCompareMode() function as the param parameter |
CTimer_B_initContinuousModeParam | Used in the Timer_B_initContinuousMode() function as the param parameter |
CTimer_B_initUpDownModeParam | Used in the Timer_B_initUpDownMode() function as the param parameter |
CTimer_B_initUpModeParam | Used in the Timer_B_initUpMode() function as the param parameter |
CTimer_B_outputPWMParam | Used in the Timer_B_outputPWM() function as the param parameter |