Used in the Timer_B_initContinuousMode() function as the param parameter. More...
#include <timer_b.h>
Data Fields | |
uint16_t | clockSource |
uint16_t | clockSourceDivider |
uint16_t | timerInterruptEnable_TBIE |
uint16_t | timerClear |
bool | startTimer |
Whether to start the timer immediately. | |
Used in the Timer_B_initContinuousMode() function as the param parameter.
uint16_t Timer_B_initContinuousModeParam::clockSource |
Selects the clock source
Valid values are:
Referenced by Timer_B_initContinuousMode().
uint16_t Timer_B_initContinuousModeParam::clockSourceDivider |
Is the divider for Clock source.
Valid values are:
Referenced by Timer_B_initContinuousMode().
uint16_t Timer_B_initContinuousModeParam::timerClear |
Decides if Timer_B clock divider, count direction, count need to be reset.
Valid values are:
Referenced by Timer_B_initContinuousMode().
uint16_t Timer_B_initContinuousModeParam::timerInterruptEnable_TBIE |
Is to enable or disable Timer_B interrupt
Valid values are:
Referenced by Timer_B_initContinuousMode().