Used in the Timer_B_initCompareMode() function as the param parameter. More...
#include <timer_b.h>
Data Fields | |
uint16_t | compareRegister |
uint16_t | compareInterruptEnable |
uint16_t | compareOutputMode |
uint16_t | compareValue |
Is the count to be compared with in compare mode. | |
Used in the Timer_B_initCompareMode() function as the param parameter.
uint16_t Timer_B_initCompareModeParam::compareInterruptEnable |
Is to enable or disable Timer_B capture compare interrupt.
Valid values are:
Referenced by Timer_B_initCompareMode().
uint16_t Timer_B_initCompareModeParam::compareOutputMode |
Specifies the output mode.
Valid values are:
Referenced by Timer_B_initCompareMode().
uint16_t Timer_B_initCompareModeParam::compareRegister |
Selects the compare register being used. Refer to datasheet to ensure the device has the compare register being used.
Valid values are:
Referenced by Timer_B_initCompareMode().