Parameter structure that should be paired with the LEA_addLongMatrix command when using LEA_invokeCommand(). More...
#include <lea.h>
Data Fields | |
uint16_t | input1 |
uint16_t | reserved1 |
uint16_t | vectorSize |
uint16_t | input2 |
uint16_t | output |
uint16_t | input1Offset |
uint16_t | input2Offset |
uint16_t | outputOffset |
Parameter structure that should be paired with the LEA_addLongMatrix command when using LEA_invokeCommand().
uint16_t LEA_addLongMatrixParams::input1 |
LEA RAM address to input1 vector containing values in signed, unsigned or IQ31 format
uint16_t LEA_addLongMatrixParams::input1Offset |
offset for input1 pointer after every 32-bit additions
uint16_t LEA_addLongMatrixParams::input2 |
LEA RAM address to input2 vector containing values in signed, unsigned or IQ31 format
uint16_t LEA_addLongMatrixParams::input2Offset |
offset for input2 pointer after every 32-bit additions
uint16_t LEA_addLongMatrixParams::output |
LEA RAM address to output vector
uint16_t LEA_addLongMatrixParams::outputOffset |
offset for output pointer after every 32-bit additions
uint16_t LEA_addLongMatrixParams::reserved1 |
reserved
uint16_t LEA_addLongMatrixParams::vectorSize |
Input vector size