Parameter structure that should be paired with the LEA_bitReverseComplexLongEven command when using LEA_invokeCommand(). More...
#include <lea.h>
Data Fields | |
uint16_t | input1 |
uint16_t | reserved1 |
uint16_t | sqrtVectorSize |
uint16_t | reserved2 |
Parameter structure that should be paired with the LEA_bitReverseComplexLongEven command when using LEA_invokeCommand().
uint16_t LEA_bitReverseComplexLongEvenParams::input1 |
LEA RAM address to input vector containing values in cplxIQ31 format
uint16_t LEA_bitReverseComplexLongEvenParams::reserved1 |
reserved
uint16_t LEA_bitReverseComplexLongEvenParams::reserved2 |
reserved
uint16_t LEA_bitReverseComplexLongEvenParams::sqrtVectorSize |
square root of vector size