Used in the EUSCI_B_I2C_initSlave() function as the param parameter. More...
#include <eusci_b_i2c.h>
Data Fields | |
uint8_t | slaveAddress |
7-bit slave address | |
uint8_t | slaveAddressOffset |
uint32_t | slaveOwnAddressEnable |
Used in the EUSCI_B_I2C_initSlave() function as the param parameter.
uint8_t EUSCI_B_I2C_initSlaveParam::slaveAddressOffset |
Own address Offset referred to- 'x' value of UCBxI2COAx.
Valid values are:
Referenced by EUSCI_B_I2C_initSlave().
uint32_t EUSCI_B_I2C_initSlaveParam::slaveOwnAddressEnable |
Selects if the specified address is enabled or disabled.
Valid values are:
Referenced by EUSCI_B_I2C_initSlave().