Parameter structure that should be paired with the LEA_deinterleaveLong command command when using LEA_invokeCommand(). More...
#include <lea.h>
Data Fields | |
uint16_t | input1 |
uint16_t | reserved1 |
uint16_t | vectorSize |
uint16_t | interleaveDepth |
uint16_t | output |
uint16_t | reserved |
Parameter structure that should be paired with the LEA_deinterleaveLong command command when using LEA_invokeCommand().
uint16_t LEA_deinterleaveLongParams::input1 |
LEA RAM address to input1 vector containing values in int32_t format
uint16_t LEA_deinterleaveLongParams::interleaveDepth |
interleave depth
uint16_t LEA_deinterleaveLongParams::output |
LEA RAM address to output vector containing values in int32_t format
uint16_t LEA_deinterleaveLongParams::reserved1 |
reserved
uint16_t LEA_deinterleaveLongParams::vectorSize |
Input vector size