Used in the Timer_A_initCaptureMode() function as the param parameter. More...
#include <timer_a.h>
Data Fields | |
uint16_t | captureRegister |
uint16_t | captureMode |
uint16_t | captureInputSelect |
uint16_t | synchronizeCaptureSource |
uint16_t | captureInterruptEnable |
uint16_t | captureOutputMode |
Used in the Timer_A_initCaptureMode() function as the param parameter.
uint16_t Timer_A_initCaptureModeParam::captureInputSelect |
Decides the Input Select
Valid values are:
Referenced by Timer_A_initCaptureMode().
uint16_t Timer_A_initCaptureModeParam::captureInterruptEnable |
Is to enable or disable timer captureComapre interrupt.
Valid values are:
Referenced by Timer_A_initCaptureMode().
uint16_t Timer_A_initCaptureModeParam::captureMode |
Is the capture mode selected.
Valid values are:
Referenced by Timer_A_initCaptureMode().
uint16_t Timer_A_initCaptureModeParam::captureOutputMode |
Specifies the output mode.
Valid values are:
Referenced by Timer_A_initCaptureMode().
uint16_t Timer_A_initCaptureModeParam::captureRegister |
Selects the Capture register being used. Refer to datasheet to ensure the device has the capture compare register being used.
Valid values are:
Referenced by Timer_A_initCaptureMode().
uint16_t Timer_A_initCaptureModeParam::synchronizeCaptureSource |
Decides if capture source should be synchronized with timer clock
Valid values are:
Referenced by Timer_A_initCaptureMode().