Parameter structure that should be paired with the LEA_mpyMatrixRow command when using LEA_invokeCommand(). More...
#include <lea.h>
Data Fields | |
uint16_t | input1 |
uint16_t | reserved1 |
uint16_t | rowSize |
uint16_t | colSize |
uint16_t | colVector |
uint16_t | output |
Parameter structure that should be paired with the LEA_mpyMatrixRow command when using LEA_invokeCommand().
uint16_t LEA_mpyMatrixRowParams::colSize |
If PxN * NxM matrix multiplication, colSize=M
uint16_t LEA_mpyMatrixRowParams::colVector |
column vector
uint16_t LEA_mpyMatrixRowParams::input1 |
LEA RAM address to input vector containing values in Q15 format
uint16_t LEA_mpyMatrixRowParams::output |
output vector
uint16_t LEA_mpyMatrixRowParams::reserved1 |
padding
uint16_t LEA_mpyMatrixRowParams::rowSize |
If PxN * NxM matrix multiplication, rowSize=N