Parameter structure that should be paired with the LEA_maxUnsignedMatrix command when using LEA_invokeCommand(). More...
#include <lea.h>
Data Fields | |
uint16_t | input1 |
uint16_t | reserved1 |
uint16_t | vectorSize |
uint16_t | input1Offset |
uint16_t | output |
uint16_t | reserved2 |
Parameter structure that should be paired with the LEA_maxUnsignedMatrix command when using LEA_invokeCommand().
uint16_t LEA_maxUnsignedMatrixParams::input1 |
LEA RAM address to input1 vector containing values in uint16_t format
uint16_t LEA_maxUnsignedMatrixParams::input1Offset |
offset for input1 pointer after every max
uint16_t LEA_maxUnsignedMatrixParams::output |
LEA RAM address to output vector which is of size two. output[0] will have max value; output[1] will have index to max value
uint16_t LEA_maxUnsignedMatrixParams::reserved1 |
reserved
uint16_t LEA_maxUnsignedMatrixParams::reserved2 |
reserved
uint16_t LEA_maxUnsignedMatrixParams::vectorSize |
Input vector size