Parameter structure that should be paired with the LEA_goertzel command when using LEA_invokeCommand(). More...
#include <lea.h>
Data Fields | |
uint16_t | input1 |
uint16_t | reserved1 |
uint16_t | vectorSize |
uint16_t | output |
int16_t | coeffCos |
int16_t | coeffSin |
Parameter structure that should be paired with the LEA_goertzel command when using LEA_invokeCommand().
int16_t LEA_goertzelParams::coeffCos |
cos coefficient
int16_t LEA_goertzelParams::coeffSin |
sin coefficient
uint16_t LEA_goertzelParams::input1 |
LEA RAM address to input vector containing values in Q15 format
uint16_t LEA_goertzelParams::output |
LEA RAM address to output vector containing values in Q15 format
uint16_t LEA_goertzelParams::reserved1 |
reserved
uint16_t LEA_goertzelParams::vectorSize |
Input vector size