Parameter structure that should be paired with the LEA_bitReverseComplexOdd command when using LEA_invokeCommand(). More...
#include <lea.h>
Data Fields | |
uint16_t | input1 |
uint16_t | reserved1 |
uint16_t | sqrtVectorSizeBy2 |
uint16_t | reserved2 |
Parameter structure that should be paired with the LEA_bitReverseComplexOdd command when using LEA_invokeCommand().
uint16_t LEA_bitReverseComplexOddParams::input1 |
LEA RAM address to input vector containing values in cplxQ15 format
uint16_t LEA_bitReverseComplexOddParams::reserved1 |
reserved
uint16_t LEA_bitReverseComplexOddParams::reserved2 |
reserved
uint16_t LEA_bitReverseComplexOddParams::sqrtVectorSizeBy2 |
square root of vector size divided by two