TI-RTOS Drivers  tidrivers_full_2_20_01_10
File List
Here is a list of all files with brief descriptions:
 ADC.hADC driver interface
 ADCBuf.hADCBuf driver interface
 ADCBufCC26XX.hADCBuf driver implementation for a CC26XX analog-to-digital converter
 ADCCC26XX.hADC driver implementation for the ADC peripheral on CC26XX
 ADCMSP432.hADC driver implementation for the ADC peripheral on MSP432
 buzzer.hPWM-based buzzer interface
 Camera.hCamera driver interface
 CameraCC3200DMA.hCamera driver implementation for a CC3200 Camera controller
 ClockP.hClock interface for the RTOS Porting Interface
 Codec1.hImplementation of TI Codec Type 1 (IMA ADPCM) encoding and decoding
 CryptoCC26XX.hCrypto driver implementation for a CC26XX Crypto controller
 DebugP.hDebug support
 diskio.h
 Display.hGeneric interface for text output
 DisplayDogm1286.h
 DisplayExt.hExtention of Display to access GrLib functionality in capable displays
 DisplayLog.h
 DisplaySharp.h
 DisplayUart.h
 EMAC.hEMAC driver interface
 EMACSnow.hEMACSnow Driver
 EMACTiva.hEMACTiva Driver
 ExtFlash.hExternal flash storage abstraction
 ff.h
 ffcio.h
 ffconf.h
 fsutils.h
 GPIO.hGPIO driver
 GPIOCC26XX.hCC26XX GPIO driver
 GPIOCC3200.hCC3200 GPIO driver
 GPIOMSP430.hMSP430 GPIO driver
 GPIOMSP432.hMSP432 GPIO driver
 GPIOTiva.hTiva GPIO driver
 GPTimerCC26XX.hGPTimer driver implementation for CC26XX/CC13XX
 grlib.h
 HwiP.hHardware Interrupt module for the RTOS Porting Interface
 I2C.hI2C driver interface
 I2CCC26XX.hI2C driver implementation for a CC26XX I2C controller
 I2CCC3200.hI2C driver implementation for a CC3200 I2C controller
 I2CEUSCIB.hI2CEUSCIB driver implementation for an EUSCIB controller
 I2CMSP432.hI2C driver implementation for the EUSCI controller on MSP432
 I2CSlave.hI2CSlave driver interface
 I2CSlaveMSP432.hI2CSlave driver implementation for the EUSCI controller on MSP432
 I2CTiva.hI2C driver implementation for a Tiva I2C controller
 I2CUSCIB.hI2CUSCIB driver implementation for a USCIB controller
 I2S.hI2S driver interface
 I2SCC3200DMA.hI2S driver implementation for a CC3200 I2S controller
 integer.h
 LCDDogm1286.hLCD driver implementation for a DOGM128W-6 LCD display
 LCDDogm1286_util.h
 List.hLinked List interface for use in drivers
 MutexP.hMutex module for the RTOS Porting Interface
 NVS.hPRELIMINARY Non-Volatile Storage Driver
 NVSCC26XX.h
 NVSCC3200.h
 NVSMSP432.h
 NVSTiva.h
 PDMCC26XX.hPDM driver implementation for a CC26XX PDM controller
 PDMCC26XX_util.hPDM utility includes helper functions for configuring the CC26XX I2S controller
 PIN.hGeneric PIN & GPIO driver
 PINCC26XX.hDevice-specific pin & GPIO driver for CC26xx family [def]
 Power.hPower manager interface
 PowerCC26XX.hPower manager interface for CC26XX
 PowerCC3200.hPower manager interface for the CC3200
 PowerMSP432.hPower manager interface for the MSP432
 PWM.hPWM driver interface
 PWMTimerCC26XX.hPWM driver implementation for CC26XX/CC13XX
 PWMTimerCC3200.hPWM driver implementation using CC3200 General Purpose Timers
 PWMTimerMSP432.hPWM driver implementation using Timer_A peripherals
 PWMTimerTiva.hPWM driver implementation using Tiva General Purpose Timers
 PWMTiva.hPWM driver implementation for Tiva PWM peripherals
 RF.hRF driver for the CC26/13xx family
 RingBuf.h
 SDHostCC3200.hSDHost driver implementation for the CC3200
 SDSPI.hSDSPI driver interface
 SDSPICC3200.hSDSPI driver implementation for a CC3200 SPI peripheral used with the SDSPI driver
 SDSPIEUSCIA.hSDSPI driver implementation for a USCI SPI peripheral used with the SDSPI driver
 SDSPIEUSCIB.hSDSPI driver implementation for a USCI SPI peripheral used with the SDSPI driver
 SDSPIMSP432.hSDSPI driver implementation using an EUSCI SPI peripheral for MSP432
 SDSPITiva.hSDSPI driver implementation for a Tiva SPI peripheral used with the SDSPI driver
 SDSPIUSCIA.hSDSPI driver implementation for a USCI SPI peripheral used with the SDSPI driver
 SDSPIUSCIB.hSDSPI driver implementation for a USCI SPI peripheral used with the SDSPI driver
 SemaphoreP.hSemaphore module for the RTOS Porting Interface
 SensorBmp280.hDriver for the Bosch BMP280 Pressure Sensor
 SensorHdc1000.hDriver for Texas Instruments HCD1000 humidity sensor
 SensorI2C.hSimple interface to the TI-RTOS driver. Also manages switching between I2C-buses
 SensorMpu9250.hDriver for the InvenSense MPU9250 Motion Processing Unit
 SensorOpt3001.hDriver for the Texas Instruments OPT3001 Optical Sensor
 SensorTagTest.hTest code for SensorTag
 SensorTmp007.hDriver for the Texas Instruments TMP007 infra-red thermopile sensor
 SensorUtil.hCommon utility code for SensorTag
 SharpGrLib.h
 SPI.hSPI driver interface
 SPICC26XXDMA.hSPI driver implementation for a CC26XX SPI controller using the UDMA controller
 SPICC3200DMA.hSPI driver implementation for a CC3200 SPI controller using the micro DMA controller
 SPIEUSCIADMA.hSPI driver implementation for a USCIA peripheral using the micro DMA controller
 SPIEUSCIBDMA.hSPI driver implementation for a USCIB peripheral using the micro DMA controller
 SPIMSP432DMA.hSPI driver implementation for a EUSCI peripheral on MSP432 using the micro DMA controller
 SPITivaDMA.hSPI driver implementation for a TivaSPIcontroller using the micro DMA controller
 SPIUSCIADMA.hSPI driver implementation for a USCIA peripheral using the micro DMA controller
 SPIUSCIBDMA.hSPI driver implementation for a USCIB peripheral using the micro DMA controller
 tirtos_config.h
 UART.hUART driver interface
 UARTCC26XX.hUART driver implementation for a CC26XX UART controller
 UARTCC3200.hUART driver implementation for a CC3200 UART controller
 UARTCC3200DMA.hUART driver implementation for a CC3200 UART controller, using the micro DMA controller
 UARTEUSCIA.hUART driver implementation for a EUSCIA peripheral
 UARTMSP432.hUART driver implementation for a EUSCIA peripheral for MSP432
 UARTTiva.hUART driver implementation for a Tiva UART controller
 UARTTivaDMA.hUART driver implementation for a Tiva UART controller thay uses DMA
 UARTUSCIA.hUART driver implementation for a USCIA peripheral
 UDMACC26XX.hUDMACC26XX driver implementation
 UDMACC3200.hUDMA driver implementation for CC3200
 UDMAMSP432.hUDMA driver implementation for MSP432
 USBMSCHFatFs.hUSBMSCHFatFs driver interface
 USBMSCHFatFsTiva.hUSBMSCHFatFs driver implementation for a Tiva USB controller used with the USBMSCHFatFs driver
 Watchdog.hWatchdog driver interface
 WatchdogCC26XX.hWatchdog driver implementation for CC13XX/CC26XX
 WatchdogCC3200.hWatchdog driver implementation for CC3200
 WatchdogMSP430.hWatchdog driver implementation for MSP430
 WatchdogMSP432.hWatchdog driver implementation for MSP432
 WatchdogTiva.hWatchdog driver implementation for Tiva
 WiFi.hWiFi driver interface
 WiFiCC3100.hWiFi driver implementation for the SimpleLink Wi-Fi CC3100 device
 WiFiCC3200.hWiFi driver implementation for the SimpleLink Wi-Fi CC3200 device
Copyright 2016, Texas Instruments Incorporated