TI-RTOS Drivers
tidrivers_full_2_20_01_10
|
LCD driver implementation for a DOGM128W-6 LCD display.
============================================================================
The LCD header file should be included in an application as follows:
This LCD driver implementation is designed to operate on a DOGM128W-6 LCD display. This display is the one used on the SmartRF06 EB (Evaluation Board). The LCD display can be written to by first writing the data to display to an internal buffer, and then sending the buffer content to the LCD display. The LCD driver will make use of the SPI driver for updating the display. The driver contains different functions for both modifying the internal buffer and for updating the display with the buffer content.
The DOGM128W-6 LCD display contains 128 pixel columns and 64 pixel rows. The (x,y) coordinate system is as described below:
* * X -----> * Y +---------------------------------------------+ * | |(0,0) PAGE 0 (127,0)| * | | PAGE 1 | * v | PAGE 2 | * | PAGE 3 | * | PAGE 4 | * | PAGE 5 | * | PAGE 6 | * |(0,63) PAGE 7 (127,63)| * +---------------------------------------------+ *
This LCD driver uses a 5x7 font, thus each character takes up 5 pixels width and 7 pixels height. Each line of text will take up one page of the display. The difference between the defined variables LCD_CHAR_WIDTH and LCD_FONT_WIDTH equals the character spacing on the LCD display.
Before using LCD:
In total the following pins are required to operate the LCD on the SmartRF06EB:
* Board_SPI0_MOSI (Serial peripheral interface, Master-Out-Slave-In, controlled by LCD driver) * Board_SPI0_MISO (Serial peripheral interface, Master-In-Slave-Out, controlled by LCD driver) * Board_SPI0_CLK (Serial peripheral interface, Clock, controlled by LCD driver) * Board_LCD_CSN (Serial peripheral interface, Chip select, controlled by LCD driver) * Board_LCD_RST (LCD reset signal, active low, controlled by LCD driver) * Board_LCD_MODE (LCD mode signal, controlled by LCD driver) * Board_3V3_EN (Enable the 3.3V domain. NOTE: Must be set by application, NOT controlled by LCD driver) *
The following SPI parameters will be fixed by the LCD driver:
The APIs in this driver serve as an interface to a typical TI-RTOS application. The specific peripheral implementations are responsible to create all the SYS/BIOS specific primitives to allow for thread-safe operation.
After LCD operation has ended:
Please refer to the SPI driver documentation for information about error handling during a SPI transaction.
If an error occurs when modifying the internal buffers, the functions are return without completing the buffer modification.
The TI-RTOS power management framework will try to put the device into the most power efficient mode whenever possible. Please see the technical reference manual for further details on each power mode.
The LCD driver makes use of the SPICC26XXDMA driver, which is setting a power constraint during transfers to keep the device out of standby. I.e. device will enter idle mode when no tasks are active. When the transfer has finished, the power constraint is released.
The LCD driver joined (at link time) to an array of LCD_Buffer structures named lcdBuffers. lcdBuffers is implemented in the application with each entry being an instance of a LCD_Buffer. The number of buffers availible must be passed as an argument to LCD_open(). Each entry in lcdBuffers contains a:
Before the LCD screen can be filled, the data to display must be written to the internal buffers. All functions called LCD_bufferxxxx are only modifying the internal buffers. To send the buffer content to the LCD display, one must use the functions LCD_update() or LCD_updatePart(). The only exception from this is the function LCD_writeLine(), which both modifies a buffer and send the content to the LCD display.
API function | Description |
---|---|
LCD_open() | Initialize LCD display and configure SPI driver |
LCD_close() | Disable LCD operation |
LCD_writeLine() | Write a string and a number to a page on the LCD display |
LCD_update() | Write the content of a LCD buffer to the display |
LCD_updatePart() | Write part of a LCD buffer to the display |
LCD_bufferClear() | Empty an entire LCD buffer |
LCD_bufferClearPage() | Empty an entire page in a LCD buffer |
LCD_bufferClearPart() | Empty part of a LCD buffer |
LCD_bufferInvert() | Invert the pixels of a part of a LCD buffer |
LCD_bufferInvertPage() | Invert the pixels of a page in a LCD buffer |
LCD_bufferPrintString() | Write a string to a LCD buffer |
LCD_bufferPrintStringAligned() | Write an aligned string to a LCD buffer |
LCD_bufferPrintInt() | Write an integer to a LCD buffer |
LCD_bufferPrintIntAligned() | Write an aligned integer to a LCD buffer |
LCD_bufferPrintFloat() | Write a floating point number to a LCD buffer |
LCD_bufferPrintFloatAligned() | Write an aligned floating point number to a LCD buffer |
LCD_bufferSetLine() | Draw a line to a LCD buffer |
LCD_bufferClearLine() | Clear a line from a LCD buffer |
LCD_bufferSetHLine() | Draw a horizontal line to a LCD buffer |
LCD_bufferClearHLine() | Clear a horizontal line from a LCD buffer |
LCD_bufferSetVLine() | Draw a vertical line to a LCD buffer |
LCD_bufferClearVLine() | Clear a vertical line from a LCD buffer |
LCD_bufferHArrow() | Draw a horizontal arrow to a LCD buffer |
LCD_bufferVArrow() | Draw a vertical arrow to a LCD buffer |
LCD_bufferSetPx() | Set a pixel in a LCD buffer |
LCD_bufferClearPx() | Clear a pixel in a LCD buffer |
LCD_bufferCopy() | Copy content of one LCD buffer into another |
LCD_setContrast() | Set the contrast of the LCD display |
The most basic use cases discribed are described below. A complete LCD example can also be found in the TI-RTOS simplelink distribution.
The LCD driver interface produces log statements if instrumentation is enabled.
Diagnostics Mask | Log details |
---|---|
Diags_USER1 | basic operations performed |
#include <xdc/std.h>
#include <ti/drivers/SPI.h>
#include <ti/sysbios/family/arm/m3/Hwi.h>
#include <ti/sysbios/knl/Semaphore.h>
Go to the source code of this file.
Data Structures | |
struct | LCD_Params |
LCD Parameters are used to with the LCD_open() call. Default values for these parameters are set using LCD_Params_init(). More... | |
struct | LCD_Command |
Format of LCD commands used by the LCD controller. More... | |
struct | LCD_Buffer |
LCD_Buffer used to store data to be printed on the LCD display. More... | |
struct | LCD_Object |
LCD Object. More... | |
struct | LCD_HWAttrs |
LCD Hardware attributes. More... | |
struct | LCD_Config |
The LCD_Config structure contains a set of pointers used to characterize the LCD driver implementation. More... | |
Macros | |
#define | ti_sysbios_family_arm_m3_Hwi__nolocalnames |
#define | LCD_PIXELS 8192 |
#define | LCD_BYTES 1024 |
#define | LCD_COLS 128 |
#define | LCD_X_MIN 0 |
#define | LCD_X_MAX (LCD_COLS-1) |
#define | LCD_ROWS 64 |
#define | LCD_Y_MIN 0 |
#define | LCD_Y_MAX (LCD_ROWS-1) |
#define | LCD_PAGES 8 |
#define | LCD_PAGE_ROWS 8 |
#define | LCD_CHAR_WIDTH 6 |
#define | LCD_FONT_WIDTH 5 |
Typedefs | |
typedef struct LCD_Config * | LCD_Handle |
A handle that is returned from a LCD_open() call. More... | |
typedef enum LCD_Align | LCD_Align |
LCD alignment enum. More... | |
typedef enum LCD_Page | LCD_Page |
LCD page enum. More... | |
typedef enum LCD_X_Limit | LCD_X_Limit |
LCD x-axis enum. More... | |
typedef enum LCD_Y_Limit | LCD_Y_Limit |
LCD y-axis enum. More... | |
typedef struct LCD_Params | LCD_Params |
LCD Parameters are used to with the LCD_open() call. Default values for these parameters are set using LCD_Params_init(). More... | |
typedef struct LCD_Command | LCD_Command |
Format of LCD commands used by the LCD controller. More... | |
typedef struct LCD_Buffer | LCD_Buffer |
LCD_Buffer used to store data to be printed on the LCD display. More... | |
typedef struct LCD_Object | LCD_Object |
LCD Object. More... | |
typedef struct LCD_HWAttrs | LCD_HWAttrs |
LCD Hardware attributes. More... | |
typedef struct LCD_Config | LCD_Config |
The LCD_Config structure contains a set of pointers used to characterize the LCD driver implementation. More... | |
Enumerations | |
enum | LCD_Align { LCD_ALIGN_LEFT, LCD_ALIGN_CENTER, LCD_ALIGN_RIGHT } |
LCD alignment enum. More... | |
enum | LCD_Page { LCD_PAGE0 = 0, LCD_PAGE1, LCD_PAGE2, LCD_PAGE3, LCD_PAGE4, LCD_PAGE5, LCD_PAGE6, LCD_PAGE7, LCD_PAGE_COUNT } |
LCD page enum. More... | |
enum | LCD_X_Limit { LCD_X_FIRST = 0, LCD_X_LAST = (LCD_COLS-1) } |
LCD x-axis enum. More... | |
enum | LCD_Y_Limit { LCD_Y_FIRST = 0, LCD_Y_LAST = (LCD_ROWS-1) } |
LCD y-axis enum. More... | |
Functions | |
void | LCD_close (LCD_Handle handle) |
Function to close the LCD instance specified by the LCD handle. More... | |
void | LCD_init (void) |
This function initializes the LCD driver module. More... | |
LCD_Handle | LCD_open (LCD_Buffer *buffers, uint8_t nBuffers, LCD_Params *params) |
Function to set up the DOGM128W-6 LCD display. More... | |
void | LCD_Params_init (LCD_Params *params) |
Function to initialize the LCD_Params struct to its defaults. More... | |
void | LCD_writeLine (LCD_Handle handle, unsigned int bufIndex, char *str, unsigned int uiValue, unsigned char ucFormat, unsigned char ucLine) |
Function that writes a string and value to a buffer and sends it to the LCD display. The written page is being cleared before it is written to. More... | |
void | LCD_update (LCD_Handle handle, unsigned int bufIndex) |
Function that writes the specified buffer to the LCD display. More... | |
void | LCD_updatePart (LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucXTo, LCD_Page iPageFrom, LCD_Page iPageTo) |
Function that sends the specified part of the given buffer to the corresponding part on the LCD. This function assumes ucXFrom <= ucXTo and iPageFrom <= iPageTo. The resolution is given in columns [0–127] and pages [0–7]. More... | |
void | LCD_bufferClear (LCD_Handle handle, unsigned int bufIndex) |
Function that empties the specified LCD buffer. More... | |
void | LCD_bufferClearPage (LCD_Handle handle, unsigned int bufIndex, LCD_Page iPage) |
This function clears the page specified by iPage in the given buffer. More... | |
void | LCD_bufferClearPart (LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucXTo, LCD_Page iPageFrom, LCD_Page iPageTo) |
This function clears the pixels in a given piece of a page. Resolution is given in coulmns [0–127] and pages [0–7]. The function assumes ucXFrom <= ucXTo and iPageFrom <= iPageTo. More... | |
void | LCD_bufferInvert (LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucYFrom, unsigned char ucXTo, unsigned char ucYTo) |
This function inverts the pixels (bits) in a given region of the specified buffer. More... | |
void | LCD_bufferInvertPage (LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucXTo, LCD_Page iPage) |
This function inverts a range of columns in the display buffer on a specified page (for example, LCD_PAGE0). This function assumes ucXFrom <= ucXTo. More... | |
void | LCD_bufferPrintString (LCD_Handle handle, unsigned int bufIndex, const char *pcStr, unsigned char ucX, LCD_Page iPage) |
Function that writes a string to the specified buffer. More... | |
void | LCD_bufferPrintStringAligned (LCD_Handle handle, unsigned int bufIndex, const char *pcStr, LCD_Align iAlignment, LCD_Page iPage) |
This function writes a string to the given buffer specified by the iAlignment argument. More... | |
void | LCD_bufferPrintInt (LCD_Handle handle, unsigned int bufIndex, int i32Number, unsigned char ucX, LCD_Page iPage) |
Function that writes an integer to the specified buffer. More... | |
void | LCD_bufferPrintIntAligned (LCD_Handle handle, unsigned int bufIndex, int i32Number, LCD_Align iAlignment, LCD_Page iPage) |
This function writes an integer to the given buffer as specified by the iAlignment argument. More... | |
void | LCD_bufferPrintFloat (LCD_Handle handle, unsigned int bufIndex, float fNumber, unsigned char ucDecimals, unsigned char ucX, LCD_Page iPage) |
This function writes a number of data type float to the given buffer at a specified column and page. Use this function instead of performing a float to c-string conversion and then using LCD_bufferPrintString(). More... | |
void | LCD_bufferPrintFloatAligned (LCD_Handle handle, unsigned int bufIndex, float fNumber, unsigned char ucDecimals, LCD_Align iAlignment, LCD_Page iPage) |
This function writes a float number to the given buffer as specified by the iAlignment argument. More... | |
void | LCD_bufferSetLine (LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucYFrom, unsigned char ucXTo, unsigned char ucYTo) |
This function draws a line in the specified buffer from (ucXFrom,ucYFrom) to (ucXTo,ucYTo). The function uses Bresenham's line algorithm. More... | |
void | LCD_bufferClearLine (LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucYFrom, unsigned char ucXTo, unsigned char ucYTo) |
This function clears a line in the specified buffer from (ucXFrom,ucYFrom) to (ucXTo,ucYTo). The function uses Bresenham's line algorithm. More... | |
void | LCD_bufferSetHLine (LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucXTo, unsigned char ucY) |
This function draws a horizontal line from (ucXFrom,ucY) to (ucXTo,ucY) into the specified buffer. More... | |
void | LCD_bufferClearHLine (LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucXTo, unsigned char ucY) |
This function clears a horizontal line from (ucXFrom,ucY) to (ucXTo,ucY) from the specified buffer. More... | |
void | LCD_bufferSetVLine (LCD_Handle handle, unsigned int bufIndex, unsigned char ucX, unsigned char ucYFrom, unsigned char ucYTo) |
This function draws a vertical line from (ucX,ucYFrom) to (ucX,ucYTo) into the specified buffer. More... | |
void | LCD_bufferClearVLine (LCD_Handle handle, unsigned int bufIndex, unsigned char ucX, unsigned char ucYFrom, unsigned char ucYTo) |
This function clears a vertical line from (ucX,ucYFrom) to (ucX,ucYTo) from the buffer specified. More... | |
void | LCD_bufferHArrow (LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucXTo, unsigned char ucY) |
This function draws a horizontal arrow from (ucXFrom,ucY) to (ucXTo,ucY) to buffer specified. The function assumes ucY to be in the range [2–61] in order for arrowhead to fit on the LCD. More... | |
void | LCD_bufferVArrow (LCD_Handle handle, unsigned int bufIndex, unsigned char ucX, unsigned char ucYFrom, unsigned char ucYTo) |
This function draws a vertical arrow from (ucX,ucYFrom) to (ucX,ucYTo) to the buffer specified. The function assumes that ucX is in the range [2–125] for the arrowhead to fit on the LCD. More... | |
void | LCD_bufferSetPx (LCD_Handle handle, unsigned int bufIndex, unsigned char ucX, unsigned char ucY) |
This function sets a pixel on (ucX,ucY). More... | |
void | LCD_bufferClearPx (LCD_Handle handle, unsigned int bufIndex, unsigned char ucX, unsigned char ucY) |
This function clears the pixel at (ucX,ucY). More... | |
void | LCD_bufferCopy (LCD_Handle handle, unsigned int fromBufIndex, unsigned int toBufIndex) |
This function copies the content of fromBufIndex to toBufIndex. More... | |
void | LCD_setContrast (LCD_Handle handle, unsigned char ucContrast) |
This Function sets the LCD contrast. More... | |
#define ti_sysbios_family_arm_m3_Hwi__nolocalnames |
#define LCD_PIXELS 8192 |
#define LCD_BYTES 1024 |
Number of bytes needed in LCD buffer
#define LCD_COLS 128 |
Number of pixel columns
#define LCD_X_MIN 0 |
First pixel on LCD x-axis
#define LCD_X_MAX (LCD_COLS-1) |
Last pixel on LCD x-axis
#define LCD_ROWS 64 |
Number of pixel rows
#define LCD_Y_MIN 0 |
First pixel on LCD y-axis
#define LCD_Y_MAX (LCD_ROWS-1) |
Last pixel on LCD y-axis
#define LCD_PAGES 8 |
#define LCD_PAGE_ROWS 8 |
Number of pixel rows per LCD page
#define LCD_CHAR_WIDTH 6 |
Space used for each character
#define LCD_FONT_WIDTH 5 |
Actual font character width
typedef struct LCD_Config* LCD_Handle |
A handle that is returned from a LCD_open() call.
LCD alignment enum.
This enumeration defines the text alignment. It is used by LCD_bufferPrintxxxAligned functions.
LCD page enum.
This enumeration defines the LCD pages. It is used by LCD_bufferxxx functions
typedef enum LCD_X_Limit LCD_X_Limit |
LCD x-axis enum.
This enumeration defines x axis limit It is used for x argument in LCD_bufferxxx functions
typedef enum LCD_Y_Limit LCD_Y_Limit |
LCD y-axis enum.
This enumeration defines y axis limit It is used for y argument in LCD_bufferxxx functions
typedef struct LCD_Params LCD_Params |
LCD Parameters are used to with the LCD_open() call. Default values for these parameters are set using LCD_Params_init().
typedef struct LCD_Command LCD_Command |
Format of LCD commands used by the LCD controller.
typedef struct LCD_Buffer LCD_Buffer |
LCD_Buffer used to store data to be printed on the LCD display.
A sample structure is shown below:
typedef struct LCD_Object LCD_Object |
LCD Object.
The application must not access any member variables of this structure!
typedef struct LCD_HWAttrs LCD_HWAttrs |
typedef struct LCD_Config LCD_Config |
The LCD_Config structure contains a set of pointers used to characterize the LCD driver implementation.
enum LCD_Align |
enum LCD_Page |
enum LCD_X_Limit |
enum LCD_Y_Limit |
void LCD_close | ( | LCD_Handle | handle | ) |
Function to close the LCD instance specified by the LCD handle.
handle | A LCD handle returned from LCD_open() |
void LCD_init | ( | void | ) |
This function initializes the LCD driver module.
LCD_Handle LCD_open | ( | LCD_Buffer * | buffers, |
uint8_t | nBuffers, | ||
LCD_Params * | params | ||
) |
Function to set up the DOGM128W-6 LCD display.
buffers | Pointer to a buffer block. |
nBuffers | Number of buffers in the buffer block. |
params | Pointer to a parameter block, if NULL it will use default values |
void LCD_Params_init | ( | LCD_Params * | params | ) |
Function to initialize the LCD_Params struct to its defaults.
Defaults values are:
params | Parameter structure to initialize |
void LCD_writeLine | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
char * | str, | ||
unsigned int | uiValue, | ||
unsigned char | ucFormat, | ||
unsigned char | ucLine | ||
) |
Function that writes a string and value to a buffer and sends it to the LCD display. The written page is being cleared before it is written to.
LCD_write will block task execution until all the data in buffer has been written to the LCD.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
str | A pointer to the string to print. |
uiValue | Value to print |
ucFormat | Base of the value to print – 2,8,16 etc. ucFormat must be between 2 and 36, where 10 means decimal base, 16 hexadecimal, 8 octal, and 2 binary. If ucFormat is zero, only the string will get printed. |
ucLine | The page to write. Must be a value from 0-7. |
void LCD_update | ( | LCD_Handle | handle, |
unsigned int | bufIndex | ||
) |
Function that writes the specified buffer to the LCD display.
LCD_update will block task execution until all the data in buffer has been written to the LCD.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
void LCD_updatePart | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
unsigned char | ucXFrom, | ||
unsigned char | ucXTo, | ||
LCD_Page | iPageFrom, | ||
LCD_Page | iPageTo | ||
) |
Function that sends the specified part of the given buffer to the corresponding part on the LCD. This function assumes ucXFrom <= ucXTo and iPageFrom <= iPageTo. The resolution is given in columns [0–127] and pages [0–7].
LCD_updatePart will block task execution until all the data has been written to the LCD.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
ucXFrom | The lowest x-position (column) to write [0–127]. |
ucXTo | The highest x-position to write [ucXFrom–127]. |
iPageFrom | The first page to write. Must be one of the following enumerated values:
|
iPageTo | The last page to write [iPageFrom–LCD_PAGE7]. |
void LCD_bufferClear | ( | LCD_Handle | handle, |
unsigned int | bufIndex | ||
) |
Function that empties the specified LCD buffer.
LCD_bufferClear will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
void LCD_bufferClearPage | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
LCD_Page | iPage | ||
) |
This function clears the page specified by iPage in the given buffer.
LCD_bufferClearPage will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
iPage | The page to clear. Must be one of the following enumerated values:
|
void LCD_bufferClearPart | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
unsigned char | ucXFrom, | ||
unsigned char | ucXTo, | ||
LCD_Page | iPageFrom, | ||
LCD_Page | iPageTo | ||
) |
This function clears the pixels in a given piece of a page. Resolution is given in coulmns [0–127] and pages [0–7]. The function assumes ucXFrom <= ucXTo and iPageFrom <= iPageTo.
LCD_bufferClearPart will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
ucXFrom | The lowest x-position (column) to be cleared [0–127]. |
ucXTo | The highest x-position to be cleared [ucXFrom–127]. |
iPageFrom | The first page cleared. Must be one of the following enumerated values:
|
iPageTo | The last page cleared [iPageFrom–LCD_PAGE7]. |
void LCD_bufferInvert | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
unsigned char | ucXFrom, | ||
unsigned char | ucYFrom, | ||
unsigned char | ucXTo, | ||
unsigned char | ucYTo | ||
) |
This function inverts the pixels (bits) in a given region of the specified buffer.
LCD_bufferInvert will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
ucXFrom | The first x-position (column) to invert [0–127]. |
ucYFrom | is the first y-position (row) to invert [0–63]. |
ucXTo | The last x-position (column) to invert [0–127]. |
ucYTo | The last y-position (row) to invert [0–63]. |
void LCD_bufferInvertPage | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
unsigned char | ucXFrom, | ||
unsigned char | ucXTo, | ||
LCD_Page | iPage | ||
) |
This function inverts a range of columns in the display buffer on a specified page (for example, LCD_PAGE0). This function assumes ucXFrom <= ucXTo.
LCD_bufferInvertPage will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
ucXFrom | The first x-position (column) to invert [0–127]. |
ucXTo | The last x-position (column) to invert [ucXFrom–127]. |
iPage | The page on which to invert. Must be one of the following enumerated values:
|
void LCD_bufferPrintString | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
const char * | pcStr, | ||
unsigned char | ucX, | ||
LCD_Page | iPage | ||
) |
Function that writes a string to the specified buffer.
LCD_bufferPrintString will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
pcStr | A pointer to the string to print. |
ucX | The x-position (column) to begin printing [0–127]. |
iPage | The page on which to print. Must be one of the following enumerated values:
|
void LCD_bufferPrintStringAligned | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
const char * | pcStr, | ||
LCD_Align | iAlignment, | ||
LCD_Page | iPage | ||
) |
This function writes a string to the given buffer specified by the iAlignment argument.
LCD_bufferPrintStringAligned will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
pcStr | A pointer to the string to print. |
iAlignment | The text alignment. Must be one of the following enumerated values:
|
iPage | The page on which to print. Must be one of the following enumerated values:
|
void LCD_bufferPrintInt | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
int | i32Number, | ||
unsigned char | ucX, | ||
LCD_Page | iPage | ||
) |
Function that writes an integer to the specified buffer.
LCD_bufferPrintInt will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
i32Number | The number to print. |
ucX | The x-position (column) to begin printing [0–127]. |
iPage | The page on which to print. Must be one of the following enumerated values:
|
void LCD_bufferPrintIntAligned | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
int | i32Number, | ||
LCD_Align | iAlignment, | ||
LCD_Page | iPage | ||
) |
This function writes an integer to the given buffer as specified by the iAlignment argument.
LCD_bufferPrintIntAligned will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
i32Number | The number to be printed. |
iAlignment | The text alignment. Must be one of the following enumerated values:
|
iPage | The page on which to print. Must be one of the following enumerated values:
|
void LCD_bufferPrintFloat | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
float | fNumber, | ||
unsigned char | ucDecimals, | ||
unsigned char | ucX, | ||
LCD_Page | iPage | ||
) |
This function writes a number of data type float to the given buffer at a specified column and page. Use this function instead of performing a float to c-string conversion and then using LCD_bufferPrintString().
LCD_bufferPrintFloat will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
fNumber | The number to print. |
ucDecimals | The number of decimals to print, MAX = 10. |
ucX | The x-position (column) to begin printing [0–127]. |
iPage | The page on which to print. Must be one of the following enumerated values:
|
void LCD_bufferPrintFloatAligned | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
float | fNumber, | ||
unsigned char | ucDecimals, | ||
LCD_Align | iAlignment, | ||
LCD_Page | iPage | ||
) |
This function writes a float number to the given buffer as specified by the iAlignment argument.
LCD_bufferPrintFloatAligned will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
fNumber | The number to be printed. |
ucDecimals | The number of decimals to be printed, MAX = 10. |
iAlignment | The text alignment. Can be one of the following enumerated values:
|
iPage | The page on which to print. Must be one of the following enumerated values:
|
void LCD_bufferSetLine | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
unsigned char | ucXFrom, | ||
unsigned char | ucYFrom, | ||
unsigned char | ucXTo, | ||
unsigned char | ucYTo | ||
) |
This function draws a line in the specified buffer from (ucXFrom,ucYFrom) to (ucXTo,ucYTo). The function uses Bresenham's line algorithm.
This function will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
ucXFrom | The start column [0–127]. |
ucXTo | The end column [0–127]. |
ucYFrom | The start row [0–63]. |
ucYTo | The end row [0–63]. |
void LCD_bufferClearLine | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
unsigned char | ucXFrom, | ||
unsigned char | ucYFrom, | ||
unsigned char | ucXTo, | ||
unsigned char | ucYTo | ||
) |
This function clears a line in the specified buffer from (ucXFrom,ucYFrom) to (ucXTo,ucYTo). The function uses Bresenham's line algorithm.
This function will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
ucXFrom | The start column [0–127]. |
ucXTo | The end column [0–127]. |
ucYFrom | The start row [0–63]. |
ucYTo | The end row [0–63]. |
void LCD_bufferSetHLine | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
unsigned char | ucXFrom, | ||
unsigned char | ucXTo, | ||
unsigned char | ucY | ||
) |
This function draws a horizontal line from (ucXFrom,ucY) to (ucXTo,ucY) into the specified buffer.
This function will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
ucXFrom | The start column [0–127]. |
ucXTo | The end column [0–127]. |
ucY | The row [0–63]. |
void LCD_bufferClearHLine | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
unsigned char | ucXFrom, | ||
unsigned char | ucXTo, | ||
unsigned char | ucY | ||
) |
This function clears a horizontal line from (ucXFrom,ucY) to (ucXTo,ucY) from the specified buffer.
This function will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
ucXFrom | The start column [0–127]. |
ucXTo | The end column [0–127]. |
ucY | The row [0–63]. |
void LCD_bufferSetVLine | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
unsigned char | ucX, | ||
unsigned char | ucYFrom, | ||
unsigned char | ucYTo | ||
) |
This function draws a vertical line from (ucX,ucYFrom) to (ucX,ucYTo) into the specified buffer.
This function will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
ucX | The x-position (column) of the line [0–127]. |
ucYFrom | The start row [0–63]. |
ucYTo | The end row [0–63]. |
void LCD_bufferClearVLine | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
unsigned char | ucX, | ||
unsigned char | ucYFrom, | ||
unsigned char | ucYTo | ||
) |
This function clears a vertical line from (ucX,ucYFrom) to (ucX,ucYTo) from the buffer specified.
This function will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
ucX | The x-position (column) of the line [0–127]. |
ucYFrom | The start row [0–63]. |
ucYTo | The end row [0–63]. |
void LCD_bufferHArrow | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
unsigned char | ucXFrom, | ||
unsigned char | ucXTo, | ||
unsigned char | ucY | ||
) |
This function draws a horizontal arrow from (ucXFrom,ucY) to (ucXTo,ucY) to buffer specified. The function assumes ucY to be in the range [2–61] in order for arrowhead to fit on the LCD.
This function will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
ucXFrom | The start column [0–127]. |
ucXTo | The end column [0–127]. |
ucY | The the y-position (row) of the arrow [2–61]. |
void LCD_bufferVArrow | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
unsigned char | ucX, | ||
unsigned char | ucYFrom, | ||
unsigned char | ucYTo | ||
) |
This function draws a vertical arrow from (ucX,ucYFrom) to (ucX,ucYTo) to the buffer specified. The function assumes that ucX is in the range [2–125] for the arrowhead to fit on the LCD.
This function will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
ucX | The the x-position (column) of the arrow [2–125]. |
ucYFrom | The start row [0–63]. |
ucYTo | The end row [0–63]. |
void LCD_bufferSetPx | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
unsigned char | ucX, | ||
unsigned char | ucY | ||
) |
This function sets a pixel on (ucX,ucY).
This function will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
ucX | The pixel x-position (column) [0–127]. |
ucY | The pixel y-position (row) [0–63]. |
void LCD_bufferClearPx | ( | LCD_Handle | handle, |
unsigned int | bufIndex, | ||
unsigned char | ucX, | ||
unsigned char | ucY | ||
) |
This function clears the pixel at (ucX,ucY).
This function will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
bufIndex | The buffer to use, specified by its index in the LCD_Buffer structure. |
ucX | The pixel x-position (column) [0–127]. |
ucY | The pixel y-position (row) [0–63]. |
void LCD_bufferCopy | ( | LCD_Handle | handle, |
unsigned int | fromBufIndex, | ||
unsigned int | toBufIndex | ||
) |
This function copies the content of fromBufIndex to toBufIndex.
This function will block task execution until all the buffer modification has finished.
handle | A LCD_Handle |
fromBufIndex | A pointer to the destination buffer. |
toBufIndex | A pointer to the target buffer. |
void LCD_setContrast | ( | LCD_Handle | handle, |
unsigned char | ucContrast | ||
) |
This Function sets the LCD contrast.
handle | A LCD_Handle |
ucContrast | The contrast value [0–63]. |