TI-RTOS Drivers  tidrivers_full_2_20_01_10
PWMTimerCC3200.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015-2016, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
68 #ifndef ti_driver_pwm_PWMTimerCC3200__include
69 #define ti_driver_pwm_PWMTimerCC3200__include
70 
71 #ifdef __cplusplus
72 extern "C" {
73 #endif
74 
75 #include <stdbool.h>
76 #include <ti/drivers/PWM.h>
77 
88 /* Add PWMTimerCC3200_STATUS_* macros here */
89 
102 /* Add PWMTimerCC3200_CMD_* macros here */
103 
106 /* PWM function table pointer */
108 
142 typedef struct PWMTimerCC3200_HWAttrsV1 {
144  uint32_t timerBaseAddr;
146  uint16_t halfTimer;
150  uint8_t pinId;
151 
153  uint32_t gpioBaseAddr;
155  uint8_t gpioPinIndex;
157 
163 typedef struct PWMTimerCC3200_Object {
165  unsigned int gpioPowerMgrId;
166  unsigned int timerPowerMgrId;
167  uint32_t duty;
168  uint32_t period;
173  bool isOpen;
175 
176 #ifdef __cplusplus
177 }
178 #endif
179 
180 #endif /* ti_driver_pwm_PWMTimerCC3200__include */
uint16_t halfTimer
Definition: PWMTimerCC3200.h:146
struct PWMTimerCC3200_Object PWMTimerCC3200_Object
PWMTimerCC3200 Object.
unsigned int gpioPowerMgrId
Definition: PWMTimerCC3200.h:165
PWM_Duty_Units
PWM duty cycle unit definitions. Refer to device specific implementation if using PWM_DUTY_COUNTS (ra...
Definition: PWM.h:237
PWM_Duty_Units dutyUnits
Definition: PWMTimerCC3200.h:169
uint8_t pinId
Definition: PWMTimerCC3200.h:150
PWM driver interface.
PWM_Period_Units
PWM period unit definitions. Refer to device specific implementation if using PWM_PERIOD_COUNTS (raw ...
Definition: PWM.h:227
uint32_t gpioBaseAddr
Definition: PWMTimerCC3200.h:153
PWMTimerCC3200 Object.
Definition: PWMTimerCC3200.h:163
bool pwmStarted
Definition: PWMTimerCC3200.h:172
The definition of a PWM function table that contains the required set of functions to control a speci...
Definition: PWM.h:331
PWM_Period_Units periodUnits
Definition: PWMTimerCC3200.h:170
unsigned int timerPowerMgrId
Definition: PWMTimerCC3200.h:166
Power notify object structure.
Definition: Power.h:112
uint32_t duty
Definition: PWMTimerCC3200.h:167
struct PWMTimerCC3200_HWAttrsV1 PWMTimerCC3200_HWAttrsV1
PWMTimerCC3200 Hardware attributes.
uint32_t period
Definition: PWMTimerCC3200.h:168
uint32_t timerBaseAddr
Definition: PWMTimerCC3200.h:144
PWM_IdleLevel idleLevel
Definition: PWMTimerCC3200.h:171
uint8_t gpioPinIndex
Definition: PWMTimerCC3200.h:155
Power_NotifyObj postNotify
Definition: PWMTimerCC3200.h:164
uint8_t pinTimerPwmMode
Definition: PWMTimerCC3200.h:148
PWMTimerCC3200 Hardware attributes.
Definition: PWMTimerCC3200.h:142
PWM_IdleLevel
Idle output level when PWM is not running (stopped / not started).
Definition: PWM.h:246
const PWM_FxnTable PWMTimerCC3200_fxnTable
bool isOpen
Definition: PWMTimerCC3200.h:173
Copyright 2016, Texas Instruments Incorporated