351 #ifndef ti_drivers_crypto_CryptoCC26XX__include
352 #define ti_drivers_crypto_CryptoCC26XX__include
361 #include <driverlib/crypto.h>
391 #define CRYPTOCC26XX_TIMEOUT 20
393 #define CRYPTOCC26XX_STATUS_SUCCESS 0
394 #define CRYPTOCC26XX_STATUS_ERROR -1
395 #define CRYPTOCC26XX_STATUS_UNDEFINEDCMD -2
397 #define CRYPTOCC26XX_OP_AES_CCM_ENCRYPT 0
398 #define CRYPTOCC26XX_OP_AES_CCM_ENCRYPT_AAD_ONLY 1
399 #define CRYPTOCC26XX_OP_AES_CCM_DECRYPT 2
400 #define CRYPTOCC26XX_OP_AES_CCM_DECRYPT_AAD_ONLY 3
401 #define CRYPTOCC26XX_OP_AES_ECB_ENCRYPT 4
402 #define CRYPTOCC26XX_OP_AES_ECB_DECRYPT 5
403 #define CRYPTOCC26XX_OP_AES_CBC_ENCRYPT 6
404 #define CRYPTOCC26XX_OP_AES_CBC_DECRYPT 7
407 #define CRYPTOCC26XX_OP_AES_CCM CRYPTOCC26XX_OP_AES_CCM_ENCRYPT
408 #define CRYPTOCC26XX_OP_AES_CCM_NOCRYPT CRYPTOCC26XX_OP_AES_CCM_ENCRYPT_AAD_ONLY
409 #define CRYPTOCC26XX_OP_AES_CCMINV CRYPTOCC26XX_OP_AES_CCM_DECRYPT
410 #define CRYPTOCC26XX_OP_AES_CCMINV_NOCRYPT CRYPTOCC26XX_OP_AES_CCM_DECRYPT_AAD_ONLY
411 #define CRYPTOCC26XX_OP_AES_ECB CRYPTOCC26XX_OP_AES_ECB_ENCRYPT
412 #define CRYPTOCC26XX_OP_AES_ECB_NOCRYPT CRYPTOCC26XX_OP_AES_ECB_DECRYPT
419 #define ti_sysbios_family_arm_m3_Hwi__nolocalnames
420 #include <ti/sysbios/family/arm/m3/Hwi.h>
421 #include <ti/sysbios/knl/Semaphore.h>
691 ti_sysbios_family_arm_m3_Hwi_Struct
hwi;
922 #undef ti_sysbios_family_arm_m3_Hwi__nolocalnames
int CryptoCC26XX_allocateKey(CryptoCC26XX_Handle handle, CryptoCC26XX_KeyLocation keyLocation, const uint32_t *keySrc)
Function that allocates key, writes key into key store RAM and returns a handle to CryptoCC26XX Key...
CryptoCC26XX Transaction.
Definition: CryptoCC26XX.h:506
Semaphore_Struct waitSem
Definition: CryptoCC26XX.h:693
CryptoCC26XX Global Configuration.
Definition: CryptoCC26XX.h:697
CryptoCC26XX_Transaction * currentTransact
Definition: CryptoCC26XX.h:681
void CryptoCC26XX_Params_init(CryptoCC26XX_Params *params)
Function to initialize the CryptoCC26XX_Params struct to its defaults.
CryptoCC26XX AES-CCM Transaction.
Definition: CryptoCC26XX.h:562
struct CryptoCC26XX_Object CryptoCC26XX_Object
CryptoCC26XX Object.
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:611
int CryptoCC26XX_close(CryptoCC26XX_Handle handle)
Function to closes a given CryptoCC26XX peripheral specified by the CryptoCC26XX handle.
void * msgOut
Definition: CryptoCC26XX.h:576
struct CryptoCC26XX_AESCCM_Transaction CryptoCC26XX_AESCCM_Transaction
CryptoCC26XX AES-CCM Transaction.
CryptoCC26XX_Transaction * tailPtr
Definition: CryptoCC26XX.h:685
CryptoCC26XX Parameters.
Definition: CryptoCC26XX.h:486
uint8_t keyIndex
Definition: CryptoCC26XX.h:613
void * msgIn
Definition: CryptoCC26XX.h:599
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:563
Definition: CryptoCC26XX.h:472
uint8_t CryptoCC26XX_Operation
CryptoCC26XX Operation Type.
Definition: CryptoCC26XX.h:462
uint8_t fieldLength
Definition: CryptoCC26XX.h:577
Definition: CryptoCC26XX.h:475
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:507
uint8_t data[]
Definition: CryptoCC26XX.h:509
Definition: CryptoCC26XX.h:439
CryptoCC26XX_Transaction * headPtr
Definition: CryptoCC26XX.h:684
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:595
int CryptoCC26XX_loadKey(CryptoCC26XX_Handle handle, int keyIndex, const uint32_t *keySrc)
Function that writes a given key into a key store.
void * msgOut
Definition: CryptoCC26XX.h:615
uint8_t keyIndex
Definition: CryptoCC26XX.h:565
char * nonce
Definition: CryptoCC26XX.h:568
void * msgOut
Definition: CryptoCC26XX.h:600
struct CryptoCC26XX_Config CryptoCC26XX_Config
CryptoCC26XX Global Configuration.
void CryptoCC26XX_Transac_init(CryptoCC26XX_Transaction *trans, CryptoCC26XX_Operation opType)
Function to initialize the CryptoCC26XX_Transaction struct to its defaults.
int CryptoCC26XX_releaseKey(CryptoCC26XX_Handle handle, int *keyIndex)
Function that releases the specified CryptoCC26XX Key.
Definition: CryptoCC26XX.h:478
char * header
Definition: CryptoCC26XX.h:575
CryptoCC26XX Hardware Attributes.
Definition: CryptoCC26XX.h:649
Power_NotifyObj cryptoNotiObj
Definition: CryptoCC26XX.h:688
int openCnt
Definition: CryptoCC26XX.h:678
ti_sysbios_family_arm_m3_Hwi_Struct hwi
Definition: CryptoCC26XX.h:691
Definition: CryptoCC26XX.h:477
void const * hwAttrs
Definition: CryptoCC26XX.h:702
uint16_t headerLength
Definition: CryptoCC26XX.h:585
Definition: CryptoCC26XX.h:445
uint16_t msgInLength
Definition: CryptoCC26XX.h:583
struct CryptoCC26XX_Params CryptoCC26XX_Params
CryptoCC26XX Parameters.
struct CryptoCC26XX_Config * CryptoCC26XX_Handle
A handle that is returned from a CryptoCC26XX_open() call.
Definition: CryptoCC26XX.h:426
void * msgIn
Definition: CryptoCC26XX.h:614
Power notify object structure.
Definition: Power.h:112
uint32_t timeout
Definition: CryptoCC26XX.h:679
Definition: CryptoCC26XX.h:479
CryptoCC26XX_Mode
CryptoCC26XX Mode Settings.
Definition: CryptoCC26XX.h:434
CryptoCC26XX AES-ECB Transaction.
Definition: CryptoCC26XX.h:610
char * msgIn
Definition: CryptoCC26XX.h:569
void CryptoCC26XX_init(void)
Function to initializes bios modules needed by CryptoCC26XX module.
uint8_t intPriority
Crypto Peripheral's interrupt priority.
Definition: CryptoCC26XX.h:668
int CryptoCC26XX_transact(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto operation (encryption or decryption) in blocking mode.
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:596
CryptoCC26XX_KeyStore keyStore
Definition: CryptoCC26XX.h:680
uint8_t keyIndex
Definition: CryptoCC26XX.h:597
uint16_t msgInLength
Definition: CryptoCC26XX.h:601
int powerMngrId
Definition: CryptoCC26XX.h:653
void * object
Definition: CryptoCC26XX.h:699
Semaphore_Struct transSem
Definition: CryptoCC26XX.h:692
Definition: CryptoCC26XX.h:480
Definition: CryptoCC26XX.h:474
uint8_t CryptoCC26XX_KeyStore
CryptoCC26XX Key.
Definition: CryptoCC26XX.h:495
CryptoCC26XX_Handle CryptoCC26XX_open(unsigned int index, bool exclusiveAccess, CryptoCC26XX_Params *params)
Function to initialize a given CryptoCC26XX peripheral specified by the particular index value...
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:612
void * nonce
Definition: CryptoCC26XX.h:598
CryptoCC26XX_KeyLocation
CryptoCC26XX Key Store Location.
Definition: CryptoCC26XX.h:470
int intNum
Definition: CryptoCC26XX.h:655
struct CryptoCC26XX_HWAttrs CryptoCC26XX_HWAttrs
CryptoCC26XX Hardware Attributes.
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:508
Definition: CryptoCC26XX.h:476
struct CryptoCC26XX_Transaction CryptoCC26XX_Transaction
CryptoCC26XX Transaction.
uint32_t timeout
Definition: CryptoCC26XX.h:487
CryptoCC26XX Object.
Definition: CryptoCC26XX.h:676
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:564
uint32_t baseAddr
Definition: CryptoCC26XX.h:651
struct CryptoCC26XX_AESECB_Transaction CryptoCC26XX_AESECB_Transaction
CryptoCC26XX AES-ECB Transaction.
struct CryptoCC26XX_AESCBC_Transaction CryptoCC26XX_AESCBC_Transaction
CryptoCC26XX AES-CBC Transaction.
Definition: CryptoCC26XX.h:473
int CryptoCC26XX_transactPolling(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto transaction operation (encryption or decryption) in polling mode...
int CryptoCC26XX_transactCallback(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto transaction operation (encryption or decryption) in callback mode...
uint8_t authLength
Definition: CryptoCC26XX.h:566
CryptoCC26XX AES-CBC Transaction.
Definition: CryptoCC26XX.h:594
Definition: CryptoCC26XX.h:471