TI-RTOS Drivers  tidrivers_full_2_20_01_10
I2CSlaveMSP432.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015-2016, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
49 #ifndef ti_drivers_i2cslave_I2CSlaveMSP432__include
50 #define ti_drivers_i2cslave_I2CSlaveMSP432__include
51 
52 #ifdef __cplusplus
53 extern "C" {
54 #endif
55 
56 #include <stdint.h>
57 #include <stdbool.h>
58 
59 #include <ti/drivers/I2CSlave.h>
60 #include <ti/drivers/ports/HwiP.h>
62 #include <ti/drivers/Power.h>
63 
64 /* I2C function table pointer */
66 
85 typedef struct I2CSlaveMSP432_HWAttrs {
86  uint32_t baseAddr;
87  uint32_t intNum;
88  uint32_t intPriority;
89  uint32_t slaveAddress;
91 
97 typedef struct I2CSlaveMSP432_Object {
98  SemaphoreP_Handle mutex; /* Grants exclusive access */
99  /* Notify finished I2C transfer */
101 
103 
104  I2CSlave_CallbackFxn transferCallbackFxn; /* Callback function pointer */
105  /* Internal inc. writeBuf index */
106  const uint8_t *writeBufferIdx;
107  /* Internal inc. readBuf index */
108  uint8_t *readBufferIdx;
109  size_t countIdx; /* Internal dec. writeCounter */
110 
111  volatile I2CSlave_Mode mode; /* Stores the I2CSlave state */
112  I2CSlave_TransferMode transferMode; /* Blocking or Callback mode */
113 
114  /* To determine if the I2CSlave is open */
115  bool isOpen;
118 
119 #ifdef __cplusplus
120 }
121 #endif
122 
123 #endif /* ti_drivers_i2cslave_I2CMSP432__include */
SemaphoreP_Handle transferComplete
Definition: I2CSlaveMSP432.h:100
I2CSlave_TransferMode
I2CSlave transfer mode.
Definition: I2CSlave.h:207
volatile I2CSlave_Mode mode
Definition: I2CSlaveMSP432.h:111
Power manager interface.
SemaphoreP_Handle mutex
Definition: I2CSlaveMSP432.h:98
void(* I2CSlave_CallbackFxn)(I2CSlave_Handle, bool)
I2CSlave callback function.
Definition: I2CSlave.h:224
I2CSlaveMSP432 Object.
Definition: I2CSlaveMSP432.h:97
uint8_t * readBufferIdx
Definition: I2CSlaveMSP432.h:108
uint32_t intNum
Definition: I2CSlaveMSP432.h:87
HwiP_Handle hwiHandle
Definition: I2CSlaveMSP432.h:102
I2CSlaveMSP432 Hardware attributes These fields are used by driverlib APIs and therefore must be popu...
Definition: I2CSlaveMSP432.h:85
void * SemaphoreP_Handle
Opaque client reference to an instance of a SemaphoreP.
Definition: SemaphoreP.h:96
I2CSlave driver interface.
Semaphore module for the RTOS Porting Interface.
uint32_t slaveAddress
Definition: I2CSlaveMSP432.h:89
struct I2CSlaveMSP432_HWAttrs I2CSlaveMSP432_HWAttrs
I2CSlaveMSP432 Hardware attributes These fields are used by driverlib APIs and therefore must be popu...
I2CSlave_Mode
I2CSlave mode.
Definition: I2CSlave.h:192
const I2CSlave_FxnTable I2CSlaveMSP432_fxnTable
I2CSlave_TransferMode transferMode
Definition: I2CSlaveMSP432.h:112
uint32_t baseAddr
Definition: I2CSlaveMSP432.h:86
bool transferInProgress
Definition: I2CSlaveMSP432.h:116
uint32_t intPriority
Definition: I2CSlaveMSP432.h:88
bool isOpen
Definition: I2CSlaveMSP432.h:115
struct I2CSlaveMSP432_Object I2CSlaveMSP432_Object
I2CSlaveMSP432 Object.
const uint8_t * writeBufferIdx
Definition: I2CSlaveMSP432.h:106
void * HwiP_Handle
Opaque client reference to an instance of a HwiP.
Definition: HwiP.h:66
I2CSlave_CallbackFxn transferCallbackFxn
Definition: I2CSlaveMSP432.h:104
Hardware Interrupt module for the RTOS Porting Interface.
The definition of a I2CSlave function table that contains the required set of functions to control a ...
Definition: I2CSlave.h:304
size_t countIdx
Definition: I2CSlaveMSP432.h:109
Copyright 2016, Texas Instruments Incorporated