Implements Data path Micro Doppler processing functionality.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Go to the source code of this file.
Data Structures | |
struct | FeatExtract_reducedFeatOutput |
struct | DPU_uDopProc_FeatureObj |
struct | DPU_uDopProc_RadarCubeChunkEdmaCfg |
Source and destination addresses for EDMA input configuration. More... | |
struct | DPU_uDopProc_InitParams |
dopplerProc DPU initial configuration parameters More... | |
struct | DPU_uDopProc_HwaParamSaveLoc |
Structure for the HWA Params save location. More... | |
struct | DPU_uDopProc_scratch |
Structure for. More... | |
struct | DPU_uDopProc_HwaCfg |
dopplerProc DPU HWA configuration parameters More... | |
struct | DPU_uDopProc_HwaMaxOutput |
Maximum peaks filled by HWA statistics block. More... | |
struct | DPU_uDopProc_HwaSumOutput |
Sum filled by HWA statistics block. More... | |
struct | DPU_uDopProc_EdmaCfg |
dopplerProc DPU EDMA configuration parameters More... | |
struct | DPU_uDopProc_HW_Resources |
Doppler DPU HW configuration parameters. More... | |
struct | DPU_uDopProc_compRxChannelBiasCfg |
Range Bias and rx channel gain/phase compensation configuration. More... | |
struct | DPU_uDopProcCliCfg |
Micro Doppler Processing CLI Configuration. More... | |
struct | DPU_uDopClassifierCliCfg |
Micro Doppler Classifier CLI Configuration. More... | |
struct | DPU_uDopProc_StaticConfig |
Doppler DPU static configuration parameters. More... | |
struct | DPU_uDopProc_Config |
dopplerProc DPU configuration parameters More... | |
struct | DPU_uDopProc_tList |
Structure holds the target coordinates. More... | |
struct | DPU_uDopProc_TrackerData |
struct | DPU_uDopProc_classifierPrediction |
struct | DPU_uDopProc_classifierOutput |
struct | DPU_uDopProc_OutParams |
DPU processing output parameters. More... | |
Typedefs | |
typedef void * | classifier_Handle |
Handle for classifier. More... | |
typedef void * | DPU_uDopProc_Handle |
Handle for Doppler Processing DPU. More... | |
Functions | |
DPU_uDopProc_Handle | DPU_uDopProc_init (DPU_uDopProc_InitParams *initCfg, int32_t *errCode) |
int32_t | DPU_uDopProc_process (DPU_uDopProc_Handle handle, DPIF_RadarCube *radarCube, DPIF_DetMatrix *detMatrix, DPU_uDopProc_TrackerData *trackerData, DPU_uDopProc_OutParams *outParams) |
int32_t | DPU_uDopProc_deinit (DPU_uDopProc_Handle handle) |
int32_t | DPU_uDopProc_config (DPU_uDopProc_Handle handle, DPU_uDopProc_Config *cfg) |
int32_t | DPU_uDopProc_GetNumUsedHwaParamSets (DPU_uDopProc_Handle handle, uint8_t *numUsedHwaParamSets) |
#define DP_ERRNO_UDOPPLER_PROC_BASE (MMWAVE_ERRNO_DPU_BASE -700) |
#define DPU_UDOPPROC_MAX_NUM_HWA_PARAMSET 6 |
Maximum number of HWA paramsets used by DPU.
#define DPU_UDOPPROC_NUM_HWA_MEMBANKS 4 |
Number of HWA memory banks needed.
#define DPU_UDOPPROC_FIRST_SCALING_DISABLED ((uint8_t)0U) |
Disables first butterfly stage scaling.
#define DPU_UDOPPROC_FIRST_SCALING_ENABLED ((uint8_t)1U) |
Enables first butterfly stage scaling.
#define DPU_UDOPPROC_RANGE_LOOP_HWA_CONTROL (0) |
Range loop type controlled by HWA.
#define DPU_UDOPPROC_RANGE_LOOP_CPU_CONTROL (1) |
Range loop type controlled by CPU.
#define DPU_UDOPPROC_MAX_NUM_TRACKS TRACKER_MAX_NUM_TR |
Maximum number of tracks.
#define DPU_UDOPPROC_AZIMUTH_FFT_APPROACH 0 |
#define DPU_UDOPPROC_AZIMUTH_BEAM_FORMING_APPROACH 1 |
#define DPU_UDOPPROC_MAX_NUM_AZIMUTH_ACCUM_BINS 15 |
#define CLASSIFIER_NUM_FRAMES 30 |
#define CLASSIFIER_NUM_FEATURES 4 |
#define CLASSIFIER_NUM_CLASSES 2 |
typedef void* classifier_Handle |
Handle for classifier.
typedef void* DPU_uDopProc_Handle |
Handle for Doppler Processing DPU.
DPU_uDopProc_Handle DPU_uDopProc_init | ( | DPU_uDopProc_InitParams * | initCfg, |
int32_t * | errCode | ||
) |
int32_t DPU_uDopProc_process | ( | DPU_uDopProc_Handle | handle, |
DPIF_RadarCube * | radarCube, | ||
DPIF_DetMatrix * | detMatrix, | ||
DPU_uDopProc_TrackerData * | trackerData, | ||
DPU_uDopProc_OutParams * | outParams | ||
) |
int32_t DPU_uDopProc_deinit | ( | DPU_uDopProc_Handle | handle | ) |
int32_t DPU_uDopProc_config | ( | DPU_uDopProc_Handle | handle, |
DPU_uDopProc_Config * | cfg | ||
) |
int32_t DPU_uDopProc_GetNumUsedHwaParamSets | ( | DPU_uDopProc_Handle | handle, |
uint8_t * | numUsedHwaParamSets | ||
) |