Base error code for the dopplerProc DPU is defined in the
#define DPU_UDOPPROC_EINVAL (DP_ERRNO_UDOPPLER_PROC_BASE-1) |
Error Code: Invalid argument.
#define DPU_UDOPPROC_ENOMEM (DP_ERRNO_UDOPPLER_PROC_BASE-2) |
Error Code: Out of memory.
#define DPU_UDOPPROC_EINPROGRESS (DP_ERRNO_UDOPPLER_PROC_BASE-3) |
Error Code: DPU is in progress.
#define DPU_UDOPPROC_EHWARES (DP_ERRNO_UDOPPLER_PROC_BASE-4) |
Error Code: Out of HWA resources.
#define DPU_UDOPPROC_ESEMA (DP_ERRNO_UDOPPLER_PROC_BASE-5) |
Error Code: Semaphore creation failed.
#define DPU_UDOPPROC_ESEMASTATUS (DP_ERRNO_UDOPPLER_PROC_BASE-6) |
Error Code: Bad semaphore status.
#define DPU_UDOPPROC_EEXCEEDHWAMEM (DP_ERRNO_UDOPPLER_PROC_BASE-7) |
Error Code: Configure parameters exceed HWA memory bank size.
#define DPU_UDOPPROC_ECUBEFORMAT (DP_ERRNO_UDOPPLER_PROC_BASE-8) |
Error Code: Unsupported radar cube format.
#define DPU_UDOPPROC_EDETMFORMAT (DP_ERRNO_UDOPPLER_PROC_BASE-9) |
Error Code: Unsupported detection matrix format.
#define DPU_UDOPPROC_EDETMSIZE (DP_ERRNO_UDOPPLER_PROC_BASE-10) |
Error Code: Insufficient detection matrix size.
#define DPU_UDOPPROC_EWINDSIZE (DP_ERRNO_UDOPPLER_PROC_BASE-11) |
Error Code: Wrong window size.
#define DPU_UDOPPROC_EHWA_PARAM_SAVE_LOC_SIZE (DP_ERRNO_UDOPPLER_PROC_BASE-12) |
Error Code: Insufficient memory to save HWA param sets.
#define DPU_UDOPPROC_EEDMA_CONFIG_FAILED (DP_ERRNO_UDOPPLER_PROC_BASE-13) |
Error Code: EDMA Configuration failed.