Doppler DPU static configuration parameters.
The structure is used to hold the static configuration parameters for the Doppler DPU. The following conditions must be satisfied:
numTxAntennas * numRxAntennas * numDopplerChirps * sizeof(cmplx16ImRe_t) <= 16 KB (one HWA memory bank) numTxAntennas * numRxAntennas * numDopplerBins * sizeof(uint16_t) <= 16 KB (one HWA memory bank)
Data Fields | |
uint8_t | numTxAntennas |
Number of transmit antennas. More... | |
uint8_t | numRxAntennas |
Number of receive antennas. More... | |
uint8_t | numVirtualAntennas |
Number of virtual antennas. More... | |
uint16_t | numRangeBins |
Number of range bins. More... | |
uint16_t | numDopplerChirps |
Number of Doppler chirps. More... | |
uint16_t | numDopplerBins |
Number of Doppler bins. More... | |
uint16_t | azimuthFftSize |
Azimuth FFT size. More... | |
uint16_t | elevationFftSize |
elevation FFT size More... | |
uint16_t | numMinorMotionChirpsPerFrame |
Number of chirps per frame for Minor Motion Detection. More... | |
uint8_t | log2NumDopplerBins |
Log2 of number of Doppler bins. More... | |
uint8_t | angleDimension |
1 - 1D: 6x1 azimuth antenna array 2 - 2D: one lower row: 4 antennas, upper row 2 antennas More... | |
bool | isDetMatrixLogScale |
Detection matrix format 0 - Linear 32-bit integer, 1 - 16-bit log2 magnitude in Q11 format. More... | |
bool | isStaticClutterRemovalEnabled |
Static Clutter Removal Cfg. More... | |
bool | isRxChGainPhaseCompensationEnabled |
Range Bias and rx channel gain/phase compensation enable flag. More... | |
DPU_uDopProc_compRxChannelBiasCfg | compRxChanCfg |
Range Bias and rx channel gain/phase compensation configuration. More... | |
float | rangeStep |
Range conversion factor for FFT range index to meters. More... | |
float | dopplerStep |
Doppler conversion factor for Doppler FFT index to m/s. More... | |
uint8_t | maxNumAzimAccumBins |
Maximum number of azimuth bins in micro-doppler accumulation. More... | |
DPU_uDopProcCliCfg | cliCfg |
CLI Configuration. More... | |
uint16_t | numAntRow |
Number of virtual antenna rows. More... | |
uint16_t | numAntCol |
Number of virtual antenna columns. More... | |
uint16_t | maxNumTracks |
Maximum number of tracks by tracker. More... | |
DPU_uDopClassifierCliCfg | microDopplerClassifierCliCfg |
Classifier CLI configuration. More... | |
uint8_t DPU_uDopProc_StaticConfig::numTxAntennas |
Number of transmit antennas.
uint8_t DPU_uDopProc_StaticConfig::numRxAntennas |
Number of receive antennas.
uint8_t DPU_uDopProc_StaticConfig::numVirtualAntennas |
Number of virtual antennas.
uint16_t DPU_uDopProc_StaticConfig::numRangeBins |
Number of range bins.
uint16_t DPU_uDopProc_StaticConfig::numDopplerChirps |
Number of Doppler chirps.
uint16_t DPU_uDopProc_StaticConfig::numDopplerBins |
Number of Doppler bins.
uint16_t DPU_uDopProc_StaticConfig::azimuthFftSize |
Azimuth FFT size.
uint16_t DPU_uDopProc_StaticConfig::elevationFftSize |
elevation FFT size
uint16_t DPU_uDopProc_StaticConfig::numMinorMotionChirpsPerFrame |
Number of chirps per frame for Minor Motion Detection.
uint8_t DPU_uDopProc_StaticConfig::log2NumDopplerBins |
Log2 of number of Doppler bins.
uint8_t DPU_uDopProc_StaticConfig::angleDimension |
1 - 1D: 6x1 azimuth antenna array 2 - 2D: one lower row: 4 antennas, upper row 2 antennas
bool DPU_uDopProc_StaticConfig::isDetMatrixLogScale |
Detection matrix format 0 - Linear 32-bit integer, 1 - 16-bit log2 magnitude in Q11 format.
bool DPU_uDopProc_StaticConfig::isStaticClutterRemovalEnabled |
Static Clutter Removal Cfg.
bool DPU_uDopProc_StaticConfig::isRxChGainPhaseCompensationEnabled |
Range Bias and rx channel gain/phase compensation enable flag.
DPU_uDopProc_compRxChannelBiasCfg DPU_uDopProc_StaticConfig::compRxChanCfg |
Range Bias and rx channel gain/phase compensation configuration.
float DPU_uDopProc_StaticConfig::rangeStep |
Range conversion factor for FFT range index to meters.
float DPU_uDopProc_StaticConfig::dopplerStep |
Doppler conversion factor for Doppler FFT index to m/s.
uint8_t DPU_uDopProc_StaticConfig::maxNumAzimAccumBins |
Maximum number of azimuth bins in micro-doppler accumulation.
DPU_uDopProcCliCfg DPU_uDopProc_StaticConfig::cliCfg |
CLI Configuration.
uint16_t DPU_uDopProc_StaticConfig::numAntRow |
Number of virtual antenna rows.
uint16_t DPU_uDopProc_StaticConfig::numAntCol |
Number of virtual antenna columns.
uint16_t DPU_uDopProc_StaticConfig::maxNumTracks |
Maximum number of tracks by tracker.
DPU_uDopClassifierCliCfg DPU_uDopProc_StaticConfig::microDopplerClassifierCliCfg |
Classifier CLI configuration.