Advanced Parameter PanelΒΆ
Note: This feature is only availabe for the CC120x devices.
The Advanced Parameter Panel is a stand-alone dialog that will be shown/hidden depending on the checkbox on the upper part of the Device Control Panel. The panel gives the user an easy access to some of the more advanced RF Parameters.
Some parameters are read-only and used to show various states. Others can be used to configure features of the RF Device.
A small description is given for each parameter. A click on the question mark on the right side of the parameter title will open a dialog with the description.
Below is screen shot of the Advanced Parameter Panel: