![Logo](ti_logo.svg) |
xWRL1432 MMWAVE-L-SDK
05.03.00
|
|
Go to the documentation of this file.
77 #include <drivers/hw_include/csl_complex_math_types.h>
79 #include <drivers/hw_include/cslr_hwa.h>
89 #define HWA_RAM_WINDOW_SIZE_IN_BYTES 1024*4
92 #define HWADRV_ADDR_TRANSLATE_CPU_TO_HWA(x) (uint32_t)((uint32_t)(x) & 0x000FFFFFU)
101 #define HWA_ERRNO_BASE (-2800)
103 #define HWA_EINVAL (HWA_ERRNO_BASE-1)
105 #define HWA_ENOINIT (HWA_ERRNO_BASE-2)
107 #define HWA_EOUTOFRANGE (HWA_ERRNO_BASE-3)
109 #define HWA_EOUTOFMEM (HWA_ERRNO_BASE-4)
111 #define HWA_ENOTSUPP (HWA_ERRNO_BASE-5)
113 #define HWA_EINUSE (HWA_ERRNO_BASE-6)
115 #define HWA_ENOTALIGNED (HWA_ERRNO_BASE-7)
117 #define HWA_EINVAL_COMMON_REGISTER_PARAMSET (HWA_ERRNO_BASE-8)
119 #define HWA_EINVAL_COMMON_REGISTER_PARAMSET_ALT (HWA_ERRNO_BASE-9)
121 #define HWA_EINVAL_COMMON_REGISTER_FFTCONFIG (HWA_ERRNO_BASE-10)
123 #define HWA_EINVAL_COMMON_REGISTER_DCEST (HWA_ERRNO_BASE-11)
125 #define HWA_EINVAL_COMMON_REGISTER_CFAR (HWA_ERRNO_BASE-12)
127 #define HWA_EINVAL_COMMON_REGISTER_INTERFERENCE (HWA_ERRNO_BASE-13)
129 #define HWA_EINVAL_COMMON_REGISTER_COMPLEXMULT (HWA_ERRNO_BASE-14)
131 #define HWA_EINVAL_COMMON_REGISTER_CHANCOMB (HWA_ERRNO_BASE-15)
133 #define HWA_EINVAL_COMMON_REGISTER_ZEROINSERT (HWA_ERRNO_BASE-16)
135 #define HWA_EINVAL_COMMON_REGISTER_ADVSTAT (HWA_ERRNO_BASE-17)
137 #define HWA_EINVAL_COMMON_REGISTER_COMPRESS (HWA_ERRNO_BASE-18)
139 #define HWA_EINVAL_COMMON_REGISTER_LOCALMAXIMUM (HWA_ERRNO_BASE-19)
141 #define HWA_EINVAL_PARAMSET_GENERALCONFIG (HWA_ERRNO_BASE - 20)
143 #define HWA_EINVAL_PARAMSET_SOURCE (HWA_ERRNO_BASE - 21)
145 #define HWA_EINVAL_PARAMSET_DEST (HWA_ERRNO_BASE - 22)
147 #define HWA_EINVAL_PARAMSET_SRCDST_ADDRESS (HWA_ERRNO_BASE - 23)
149 #define HWA_EINVAL_PARAMSET_FFTMODE_GENERALCONFIG (HWA_ERRNO_BASE - 24)
151 #define HWA_EINVAL_PARAMSET_FFTMODE_SIZE (HWA_ERRNO_BASE - 25)
153 #define HWA_EINVAL_PARAMSET_FFTMODE_POSTPROC (HWA_ERRNO_BASE - 26)
155 #define HWA_EINVAL_PARAMSET_FFTMODE_PREPROC (HWA_ERRNO_BASE - 27)
157 #define HWA_EINVAL_PARAMSET_FFTMODE_PREPROC_INTERF (HWA_ERRNO_BASE - 28)
159 #define HWA_EINVAL_PARAMSET_FFTMODE_PREPROC_COMPLEXMULT (HWA_ERRNO_BASE - 29)
161 #define HWA_EINVAL_PARAMSET_CFARMODE_GENERALCONFIG (HWA_ERRNO_BASE - 30)
163 #define HWA_EINVAL_PARAMSET_CFARMODE_OSCONFIG (HWA_ERRNO_BASE - 31)
165 #define HWA_EINVAL_PARAMSET_CFARMODE_CACONFIG (HWA_ERRNO_BASE - 32)
167 #define HWA_EINVAL_PARAMSET_COMPRESSMODE (HWA_ERRNO_BASE - 33)
169 #define HWA_EINVAL_PARAMSET_LOCALMAXMODE (HWA_ERRNO_BASE - 34)
171 #define HWA_PARAMSET_POLLINGNOTALLOWED (HWA_ERRNO_BASE - 35)
175 #define HWA_NUM_RXCHANNELS (12U)
177 #define HWA_NUM_INTERFMITG_WINARRAY (5U)
179 #define HWA_BPMPATTERN_LENGTH_INWORDS (8U)
181 #define HWA_CHANCOMB_LENGTH_INWORDS (8U)
183 #define HWA_ZEROINSERT_LENGTH_INWORDS (8U)
185 #define HWA_NUM_RAMS (3U)
187 #define HWA_MAXNUM_LOOPS (4095U)
189 #define HWA_CMP_K_ARR_LEN (8U)
204 #define HWA_DONE_INTERRUPT_PRIORITY (1U)
208 #define HWA_PARAMSETDONE_INTERRUPT1_PRIORITY (1U)
210 #define HWA_PARAMSETDONE_INTERRUPT2_PRIORITY (1U)
218 #define HWA_FEATURE_BIT_ENABLE ((uint8_t)1U)
219 #define HWA_FEATURE_BIT_DISABLE ((uint8_t)0U)
227 #define HWA_SAMPLES_WIDTH_16BIT ((uint8_t)0U)
228 #define HWA_SAMPLES_WIDTH_32BIT ((uint8_t)1U)
236 #define HWA_SAMPLES_FORMAT_COMPLEX ((uint8_t)0U)
237 #define HWA_SAMPLES_FORMAT_REAL ((uint8_t)1U)
245 #define HWA_SAMPLES_UNSIGNED ((uint8_t)0U)
246 #define HWA_SAMPLES_SIGNED ((uint8_t)1U)
254 #define HWA_FFT_WINDOW_NONSYMMETRIC ((uint8_t)0U)
255 #define HWA_FFT_WINDOW_SYMMETRIC ((uint8_t)1U)
267 #define HWA_FFT_WINDOW_INTERPOLATE_MODE_NONE ((uint8_t)0U)
268 #define HWA_FFT_WINDOW_INTERPOLATE_MODE_4K ((uint8_t)1U)
269 #define HWA_FFT_WINDOW_INTERPOLATE_MODE_2K ((uint8_t)2U)
277 #define HWA_FFT_MODE_MAGNITUDE_LOG2_DISABLED ((uint8_t)0U)
278 #define HWA_FFT_MODE_MAGNITUDE_ONLY_ENABLED ((uint8_t)2U)
279 #define HWA_FFT_MODE_MAGNITUDE_LOG2_ENABLED ((uint8_t)3U)
287 #define HWA_FFT_MODE_OUTPUT_DEFAULT ((uint8_t)0U)
288 #define HWA_FFT_MODE_OUTPUT_MAX_STATS ((uint8_t)2U)
289 #define HWA_FFT_MODE_OUTPUT_SUM_STATS ((uint8_t)3U)
297 #define HWA_NOISE_AVG_MODE_CFAR_CA ((uint8_t)0U)
298 #define HWA_NOISE_AVG_MODE_CFAR_CAGO ((uint8_t)1U)
299 #define HWA_NOISE_AVG_MODE_CFAR_CASO ((uint8_t)2U)
300 #define HWA_NOISE_AVG_MODE_CFAR_OS ((uint8_t)3U)
308 #define HWA_TRIG_MODE_IMMEDIATE ((uint8_t)0U)
309 #define HWA_TRIG_MODE_SOFTWARE ((uint8_t)1U)
310 #define HWA_TRIG_MODE_RESERVED1 ((uint8_t)2U)
311 #define HWA_TRIG_MODE_DMA ((uint8_t)3U)
312 #define HWA_TRIG_MODE_HARDWARE ((uint8_t)4U)
313 #define HWA_TRIG_MODE_RESERVED2 ((uint8_t)5U)
314 #define HWA_TRIG_MODE_RESERVED3 ((uint8_t)6U)
315 #define HWA_TRIG_MODE_M4CONTROL ((uint8_t)7U)
323 #define HWA_ACCELMODE_FFT ((uint8_t)0U)
324 #define HWA_ACCELMODE_CFAR ((uint8_t)1U)
325 #define HWA_ACCELMODE_COMPRESS ((uint8_t)2U)
326 #define HWA_ACCELMODE_NONE ((uint8_t)7U)
346 #define HWA_CFAR_OPER_MODE_LOG_INPUT_REAL 0U
347 #define HWA_CFAR_OPER_MODE_LOG_INPUT_COMPLEX 1U
348 #define HWA_CFAR_OPER_MODE_MAG_INPUT_REAL 2U
349 #define HWA_CFAR_OPER_MODE_MAG_INPUT_COMPLEX 3U
350 #define HWA_CFAR_OPER_MODE_MAG_SQR_INPUT_REAL 4U
351 #define HWA_CFAR_OPER_MODE_MAG_SQR_INPUT_COMPLEX 5U
369 #define HWA_CFAR_OUTPUT_MODE_I_nAVG_ALL_Q_CUT ((uint8_t)0U)
371 #define HWA_CFAR_OUTPUT_MODE_I_nAVG_ALL_Q_DET_FLAG ((uint8_t)1U)
373 #define HWA_CFAR_OUTPUT_MODE_I_PEAK_IDX_Q_NEIGHBOR_NOISE_VAL ((uint8_t)2U)
375 #define HWA_CFAR_OUTPUT_MODE_I_PEAK_IDX_Q_CUT ((uint8_t)3U)
391 #define HWA_CMP_DCMP_COMPRESS ((uint8_t)0U)
392 #define HWA_CMP_DCMP_DECOMPRESS ((uint8_t)1U)
401 #define HWA_CMP_K_ARR_LEN (8U)
413 #define HWA_COMPRESS_METHOD_EGE ((uint8_t)0U)
429 #define HWA_COMPRESS_PATHSELECT_BOTHPASSES ((uint8_t)3U)
437 #define HWA_RAM_TYPE_WINDOW_RAM ((uint8_t)0U)
438 #define HWA_RAM_TYPE_INTERNAL_RAM ((uint8_t)1U)
447 #define HWA_ACCUMULATORREG_TYPE_DC ((uint8_t)0U)
448 #define HWA_ACCUMULATORREG_TYPE_INTERF_MAG ((uint8_t)1U)
449 #define HWA_ACCUMULATORREG_TYPE_INTERF_MAGDIFF ((uint8_t)2U)
450 #define HWA_ACCUMULATORREG_TYPE_INTERF ((uint8_t)3U)
458 #define HWA_INTERFERENCE_THRESHOLD_TYPE_MAG ((uint8_t)0U)
459 #define HWA_INTERFERENCE_THRESHOLD_TYPE_MAGDIFF ((uint8_t)1U)
469 #define HWA_PARAMDONE_INTERRUPT_TYPE_CPU ((uint8_t)1U)
470 #define HWA_PARAMDONE_INTERRUPT_TYPE_DMA ((uint8_t)2U)
479 #define HWA_COMMONCONFIG_MASK_NUMLOOPS 0x00000001
480 #define HWA_COMMONCONFIG_MASK_PARAMSTARTIDX 0x00000002
481 #define HWA_COMMONCONFIG_MASK_PARAMSTOPIDX 0x00000004
482 #define HWA_COMMONCONFIG_MASK_FFT1DENABLE 0x00000008
483 #define HWA_COMMONCONFIG_MASK_BPMRATE 0x00000010
484 #define HWA_COMMONCONFIG_MASK_BPMPATTERN 0x00000020
485 #define HWA_COMMONCONFIG_MASK_INTERFERENCETHRESHOLD 0x00000040
486 #define HWA_COMMONCONFIG_MASK_TWIDDITHERENABLE 0x00000080
487 #define HWA_COMMONCONFIG_MASK_LFSRSEED 0x00000100
488 #define HWA_COMMONCONFIG_MASK_FFTSUMDIV 0x00000200
489 #define HWA_COMMONCONFIG_MASK_CFARTHRESHOLDSCALE 0x00000400
490 #define HWA_COMMONCONFIG_MASK_I_CMULT_SCALE 0x00001000
491 #define HWA_COMMONCONFIG_MASK_Q_CMULT_SCALE 0x00002000
492 #define HWA_COMMONCONFIG_MASK_DCEST_SCALESHIFT 0x00004000
493 #define HWA_COMMONCONFIG_MASK_DCSUB_SWVAL 0x00008000
494 // #define HWA_COMMONCONFIG_MASK_INTERFMAG_THRESHOLD ((uint64_t)0x00000400U)
495 // #define HWA_COMMONCONFIG_MASK_INTERFMAGDIFF_THRESHOLD ((uint64_t)0x00000800U)
496 // #define HWA_COMMONCONFIG_MASK_INTERFSUM_MAG ((uint64_t)0x00001000U)
497 // #define HWA_COMMONCONFIG_MASK_INTERFSUM_MAGDIFF ((uint64_t)0x00002000U)
498 // #define HWA_COMMONCONFIG_MASK_COMPLEXMULT_SCALEARRAY ((uint64_t)0x00004000U)
501 // #define HWA_COMMONCONFIG_MASK_COMPLEXMULT_SCALECONST ((uint64_t)0x00008000U)
504 // #define HWA_COMMONCONFIG_MASK_INTERF_MITG_WINDOW_PARAM ((uint64_t)0x40000000U)
505 #define HWA_COMMONCONFIG_MASK_EGECOMRESS_KPARAM 0x00004000
514 #define HWA_COMPLEX_MULTIPLY_MODE_DISABLE ((uint8_t)0U)
515 #define HWA_COMPLEX_MULTIPLY_MODE_FREQ_SHIFTER ((uint8_t)1U)
516 #define HWA_COMPLEX_MULTIPLY_MODE_SLOW_DFT ((uint8_t)2U)
517 #define HWA_COMPLEX_MULTIPLY_MODE_FFT_STITCHING ((uint8_t)3U)
518 #define HWA_COMPLEX_MULTIPLY_MODE_MAG_SQUARED ((uint8_t)4U)
519 #define HWA_COMPLEX_MULTIPLY_MODE_SCALAR_MULT ((uint8_t)5U)
520 #define HWA_COMPLEX_MULTIPLY_MODE_VECTOR_MULT ((uint8_t)6U)
521 #define HWA_COMPLEX_MULTIPLY_MODE_VECTOR_MULT_2 ((uint8_t)7U)
530 #define HWA_DCEST_INTERFSUM_RESET_MODE_NOUPDATE ((uint8_t)0U)
531 #define HWA_DCEST_INTERFSUM_RESET_MODE_SOFTWARERESET ((uint8_t)1U)
532 #define HWA_DCEST_INTERFSUM_RESET_MODE_PARAMRESET ((uint8_t)2U)
533 #define HWA_DCEST_INTERFSUM_RESET_MODE_PARAMRESET_ZEROLPCONT ((uint8_t)3U)
541 #define HWA_DCSUB_SELECT_DCSW ((uint8_t)0U)
542 #define HWA_DCSUB_SELECT_DCEST ((uint8_t)1U)
551 #define HWA_FFT_STITCHING_TWID_PATTERN_2K ((uint8_t)0U)
552 #define HWA_FFT_STITCHING_TWID_PATTERN_4K ((uint8_t)1U)
588 typedef struct HWA_Attrs_t {
611 typedef struct HWA_RAMAttrs_t
628 typedef struct HWA_SrcDMAConfig_t {
642 typedef struct HWA_CommonConfig_t {
666 uint32_t bpmPattern[2];
783 } complexMultiplyConfig;
817 typedef struct HWA_SourceConfig_t {
888 typedef struct HWA_DestConfig_t {
943 typedef struct HWA_AccelModeFFT_t{
999 typedef struct HWA_AccelModeCompress_t{
1037 typedef struct HWA_ComplexMultiply_t {
1073 typedef struct HWA_PreProcessing_t {
1156 typedef struct HWA_AccelModeCFAR_t{
1204 typedef struct HWA_ParamConfig_t {
1234 typedef struct HWA_InterruptConfig_t {
1257 typedef struct HWA_Stats_t {
1272 typedef struct HWA_DebugStats_t {
1291 typedef struct HWA_MemInfo_t {
1301 typedef struct HWA_InterruptPriority_t {
1314 typedef struct HWA_OpenConfig_t {
1345 typedef struct HWA_InterruptCtx_t {
1358 typedef struct HWA_DoneInterruptCtx_t {
1367 typedef struct HWA_Driver_t {
int32_t HWA_disableDoneInterrupt(HWA_Handle handle)
Function to disable the CPU interrupt after all programmed paramSets have been completed.
uint64_t interrupt1ParamSetMask
interrupt enable mask for background thread
Definition: hwa/v0/hwa.h:1421
uint32_t refCnt
HWA instance reference (open) count.
Definition: hwa/v0/hwa.h:1375
HWA Paramset Config for Input Formatter/Source block.
Definition: hwa/v0/hwa.h:817
uint32_t destAddr
Definition: hwa/v0/hwa.h:630
int32_t HWA_readInterfThreshReg(HWA_Handle handle, uint32_t *pbuf, uint8_t startIdx, uint8_t size, uint8_t type)
Function to read the interference statistics INTF_LOC_THRESH_MAG_VAL or INTF_LOC_THRESH_MAG_VAL regis...
int32_t HWA_enable(HWA_Handle handle, uint8_t flagEnDis)
Function to enable the state machine of the HWA. This should be called after paramset and RAM have be...
int32_t HWA_reset(HWA_Handle handle)
Function to reset the internal state machine of the HWA.
uint8_t numNoiseSamplesRight
Definition: hwa/v0/hwa.h:1162
uint16_t startFreq
Definition: hwa/v0/hwa.h:1048
uint8_t nAvgDivFactor
Definition: hwa/v0/hwa.h:1169
void(* HWA_Done_IntHandlerFuncPTR)(void *arg)
HWA Interrupt callback function after all paramsets completion.
Definition: hwa/v0/hwa.h:580
uint8_t peakGroupEn
Definition: hwa/v0/hwa.h:1183
HWA Paramset Config for FFT block.
Definition: hwa/v0/hwa.h:943
uint8_t srcConjugate
Definition: hwa/v0/hwa.h:855
int32_t HWA_setDMA2ACCManualTrig(HWA_Handle handle, uint8_t idx)
Function to manually trigger the execution of the state machine waiting on DMA via software.
uint16_t maxIndex
Definition: hwa/v0/hwa.h:1259
uint16_t dstSkipInit
Definition: hwa/v0/hwa.h:931
int32_t HWA_clearDebugReg(HWA_Handle handle)
Function to clear the debug registers (acc_trig_in_clr)
HWA Local memory Information.
Definition: hwa/v0/hwa.h:1291
uint8_t dmaTriggerSrc
Definition: hwa/v0/hwa.h:1207
uint32_t iSumLSB
Definition: hwa/v0/hwa.h:1262
uint32_t gHwaConfigNum
Externally defined driver configuration array size.
uint32_t srcAddr
Definition: hwa/v0/hwa.h:629
HWA_Handle HWA_open(uint32_t index, HWA_OpenConfig *hwaCfg, int32_t *errCode)
Function to initialize HWA specified by the particular index value.
uint16_t bankSize
Definition: hwa/v0/hwa.h:1293
uint8_t bpmEnable
Definition: hwa/v0/hwa.h:872
uint8_t passSelect
Definition: hwa/v0/hwa.h:1012
int32_t HWA_getDMAChanIndex(HWA_Handle handle, uint8_t edmaChanId, uint8_t *hwaDestChan)
Function to get the dma destination index with a given EDMA channel number This function assumes the ...
int32_t HWA_enableParamSetInterrupt(HWA_Handle handle, uint8_t paramsetIdx, HWA_InterruptConfig *intrConfig)
Function to enable the CPU and/or DMA interrupt after a paramSet completion. The CPU interrupt for ev...
int32_t HWA_enableDoneInterrupt(HWA_Handle handle, HWA_Done_IntHandlerFuncPTR callbackFn, void *callbackArg)
Function to enable the CPU interrupt after all programmed paramSets have been completed in the backgr...
uint8_t shift
Definition: hwa/v0/hwa.h:692
uint32_t backgroundDone
HWA interrupt priority for the background thread done.
Definition: hwa/v0/hwa.h:1303
uint8_t headerEnable
Definition: hwa/v0/hwa.h:1015
HWA Paramset Config for ComplexMultiply block.
Definition: hwa/v0/hwa.h:1037
HWA_AccelModeFFT fftMode
Definition: hwa/v0/hwa.h:1218
uint8_t srcWidth
Definition: hwa/v0/hwa.h:846
uint32_t intNumDone
Definition: hwa/v0/hwa.h:596
uint32_t baseAddress
Definition: hwa/v0/hwa.h:1292
HWA Paramset Config for CFAR block.
Definition: hwa/v0/hwa.h:1156
uint32_t numHwaParamSets
Definition: hwa/v0/hwa.h:594
uint8_t dstChannel
Definition: hwa/v0/hwa.h:1246
uint8_t method
Definition: hwa/v0/hwa.h:1005
uint16_t dstAddr
Definition: hwa/v0/hwa.h:889
uint16_t numLoops
Definition: hwa/v0/hwa.h:646
uint8_t dstConjugate
Definition: hwa/v0/hwa.h:917
uint32_t paramsetDone1
HWA interrupt priority for paramset done interrupt 1.
Definition: hwa/v0/hwa.h:1305
uint8_t freqIncrement
Definition: hwa/v0/hwa.h:1051
uint8_t compressDecompress
Definition: hwa/v0/hwa.h:1000
void HWA_init(void)
Function to initialize the HWA module.
HWA_Attrs gHwaAttrs[]
Externally defined driver configuration array.
volatile uint32_t ctrlBaseAddr
Definition: hwa/v0/hwa.h:590
HWA configuration structure, which describes the configuration information, needed for hwa handle ope...
Definition: hwa/v0/hwa.h:1314
bool isConcurrentAccessAllowed
Definition: hwa/v0/hwa.h:600
uint8_t interruptTypeFlag
Definition: hwa/v0/hwa.h:1235
uint16_t cCnt
Definition: hwa/v0/hwa.h:633
HWA_InterruptPriority interruptPriority
structure holds the HWA interrupt priorities. This structure is applicable for processors that suppor...
Definition: hwa/v0/hwa.h:1316
uint8_t paramStartIdx
Definition: hwa/v0/hwa.h:649
uint8_t dstWidth
Definition: hwa/v0/hwa.h:908
uint8_t twidDitherEnable
Definition: hwa/v0/hwa.h:674
int32_t HWA_getCfarPeakCntRegAddress(HWA_Handle handle, uint32_t *peakCntAddr)
Function to get the address of CFAR Peak Count register.
uint8_t dfePingPongStatus
Definition: hwa/v0/hwa.h:1281
uint8_t dcSubEnable
Definition: hwa/v0/hwa.h:1080
int32_t HWA_getDMAconfig(HWA_Handle handle, uint8_t dmaTriggerSrc, HWA_SrcDMAConfig *dmaConfig)
Function to get the config to program the DMA for a given DMA Trigger channel. Application should use...
uint16_t paramSetMapInProgress
HWA paramset config is in progress [used as bitmap]. Protects Paramset register access in HWA_configP...
Definition: hwa/v0/hwa.h:1386
HWA Debug statistics.
Definition: hwa/v0/hwa.h:1272
int32_t HWA_readInterfFrameCountReg(HWA_Handle handle, uint32_t *numInterfSamplesFrame)
Function to read the number of samples that exceeded the threshold in a frame.
uint8_t numNoiseSamplesLeft
Definition: hwa/v0/hwa.h:1157
HwiP_Object hwiHandleParamSet
Registered Interrupt Handler for each paramset completion.
Definition: hwa/v0/hwa.h:1395
uint8_t qSumMSB
Definition: hwa/v0/hwa.h:1261
uint8_t fft1DEnable
Definition: hwa/v0/hwa.h:657
int32_t HWA_close(HWA_Handle handle)
Function to close a HWA peripheral specified by the HWA handle.
uint8_t triggerMode
Definition: hwa/v0/hwa.h:1205
uint8_t currentParamSet
Definition: hwa/v0/hwa.h:1273
int32_t HWA_readCFARPeakCountReg(HWA_Handle handle, uint8_t *pbuf, uint8_t size)
Function to read the PEAKCNT register.
uint8_t cyclicModeEn
Definition: hwa/v0/hwa.h:1191
void * callbackArg
Definition: hwa/v0/hwa.h:1361
uint8_t paramStopIdx
Definition: hwa/v0/hwa.h:652
HWA_ParamDone_IntHandlerFuncPTR callbackFn
Definition: hwa/v0/hwa.h:1242
uint8_t dcEstResetMode
Definition: hwa/v0/hwa.h:1075
DSSHWACCPARAMRegs * HWA_getParamSetAddr(HWA_Handle handle, uint8_t paramsetIdx)
Function to returns the HWA paramSet base address.
int32_t HWA_readDCAccReg(HWA_Handle handle, cmplx64ImRe_t *accbuf, uint8_t startIdx, uint8_t size)
Function to read the DC estimation accumulator register,.
volatile uint32_t accelMemBaseAddr
Definition: hwa/v0/hwa.h:598
uint16_t butterflyScaling
Definition: hwa/v0/hwa.h:953
int32_t HWA_getEDMAChanId(HWA_Handle handle, uint8_t hwaDMAdestChan)
Function to get the edma EDMA channel number from a given HWA paramset destination channel....
uint16_t aCnt
Definition: hwa/v0/hwa.h:631
HWA_InterruptCtx * interruptCtxParamSet
Registered Interrupt Handler for each paramset completion in the ALT thread.
Definition: hwa/v0/hwa.h:1416
uint8_t nAvgMode
Definition: hwa/v0/hwa.h:1175
HWA_ParamDone_IntHandlerFuncPTR callbackFn
Definition: hwa/v0/hwa.h:1346
int16_t srcBIdx
Definition: hwa/v0/hwa.h:832
uint8_t fftEn
Definition: hwa/v0/hwa.h:944
uint16_t dmaTrigStatus
Definition: hwa/v0/hwa.h:1280
HwiP_Object hwiHandleDone
Registered Interrupt Handler for interrupt at the end of group of paramsets.
Definition: hwa/v0/hwa.h:1400
DSSHWACCRegs * HWA_getCommonCtrlAddr(HWA_Handle handle)
Function to returns the HWA common control base address.
volatile uint32_t ramBaseAddr
Definition: hwa/v0/hwa.h:592
uint8_t EGEKarrayLength
Definition: hwa/v0/hwa.h:1026
HWA_RAMAttrs gHwaRamCfg[HWA_NUM_RAMS]
Externally defined driver RAM configuration array.
HWA_AccelModeCFAR cfarMode
Definition: hwa/v0/hwa.h:1219
HWA Paramset Config for pre-processing block.
Definition: hwa/v0/hwa.h:1073
uint32_t ramSizeInBytes
Definition: hwa/v0/hwa.h:614
uint16_t srcBcnt
Definition: hwa/v0/hwa.h:830
uint8_t dcSubSelect
Definition: hwa/v0/hwa.h:1084
uint8_t operMode
Definition: hwa/v0/hwa.h:1178
uint8_t interfZeroOutEn
Definition: hwa/v0/hwa.h:959
uint32_t interferenceThreshold
Definition: hwa/v0/hwa.h:669
uint8_t fftSumDiv
Definition: hwa/v0/hwa.h:680
int32_t HWA_configCommon(HWA_Handle handle, HWA_CommonConfig *commonConfig)
Function to set the common HWA configuration parameters needed for the next operations/iterations/par...
#define HWA_NUM_RXCHANNELS
Number of RX channels in pre-processing block.
Definition: hwa/v0/hwa.h:175
uint32_t configMask
Definition: hwa/v0/hwa.h:643
uint8_t swTrigStatus
Definition: hwa/v0/hwa.h:1282
uint32_t numDmaChannels
Definition: hwa/v0/hwa.h:597
int32_t HWA_getHWAMemInfo(HWA_Handle handle, HWA_MemInfo *memInfo)
Function to get HWA processing Memory information including address, size and number of banks.
HWA_Object gHwaObject[]
Externally defined driver object.
int32_t HWA_configRam(HWA_Handle handle, uint8_t ramType, uint8_t *data, uint32_t dataSize, uint32_t startIdx)
Function to set the HWA RAM : HWA_RAM_TYPE_WINDOW_RAM, HWA_RAM_TYPE_VECTORMULTIPLY_RAM,...
uint8_t winSymm
Definition: hwa/v0/hwa.h:972
uint8_t srcSign
Definition: hwa/v0/hwa.h:849
HWA interrupt priority for HWA background thread done, ALT thread done, paramset done interrupt 1 and...
Definition: hwa/v0/hwa.h:1301
uint8_t srcScale
Definition: hwa/v0/hwa.h:863
void(* HWA_ParamDone_IntHandlerFuncPTR)(uint32_t paramSet, void *arg)
HWA Interrupt callback function after every paramset completion.
Definition: hwa/v0/hwa.h:572
HWA_AccelModeCompress compressMode
Definition: hwa/v0/hwa.h:1220
uint8_t magLogEn
Definition: hwa/v0/hwa.h:981
uint32_t accelMemSize
Definition: hwa/v0/hwa.h:599
int32_t HWA_configParamSet(HWA_Handle handle, uint8_t paramsetIdx, HWA_ParamConfig *paramConfig, HWA_SrcDMAConfig *dmaConfig)
Function to set the HWA configuration parameters for a given paramSet.
uint8_t srcRealComplex
Definition: hwa/v0/hwa.h:843
uint8_t numGuardCells
Definition: hwa/v0/hwa.h:1167
HWA Interrupt Config.
Definition: hwa/v0/hwa.h:1234
uint16_t twidIncrement
Definition: hwa/v0/hwa.h:1042
uint8_t iSumMSB
Definition: hwa/v0/hwa.h:1260
Source trigger DMA parameters.
Definition: hwa/v0/hwa.h:628
uint8_t mode
Definition: hwa/v0/hwa.h:1038
uint32_t ramBaseAddress
Definition: hwa/v0/hwa.h:613
HWA Interrupt context structure for done interrupt.
Definition: hwa/v0/hwa.h:1358
uint8_t fftOutMode
Definition: hwa/v0/hwa.h:984
uint32_t q_cmult_scale
Definition: hwa/v0/hwa.h:799
volatile uint32_t paramBaseAddr
Definition: hwa/v0/hwa.h:591
uint16_t windowStart
Definition: hwa/v0/hwa.h:967
HWA Common Config.
Definition: hwa/v0/hwa.h:642
HWA_DestConfig dest
Definition: hwa/v0/hwa.h:1216
volatile uint32_t dssBaseAddr
Definition: hwa/v0/hwa.h:593
void * callbackArg
Definition: hwa/v0/hwa.h:1347
uint8_t dstSign
Definition: hwa/v0/hwa.h:911
int16_t twiddleDeltaFrac
Definition: hwa/v0/hwa.h:772
#define HWA_CMP_K_ARR_LEN
The length of EGE compression/decompression K-paramseters array.
Definition: hwa/v0/hwa.h:401
int32_t HWA_disableParamSetInterrupt(HWA_Handle handle, uint8_t paramsetIdx, uint8_t interruptTypeFlag)
Function to disable the CPU and/or DMA interrupt after a paramSet completion.
uint8_t configInProgress
HWA instance config is in progress. Protects Common register acccess in HWA_configCommon() and HWA_co...
Definition: hwa/v0/hwa.h:1380
uint16_t bpmRate
Definition: hwa/v0/hwa.h:663
uint32_t cfarThresholdScale
Definition: hwa/v0/hwa.h:787
Opaque Hwi object used with the Hwi APIs.
Definition: HwiP.h:91
uint8_t recWindowReset
Definition: hwa/v0/hwa.h:780
uint8_t winInterpolateMode
Definition: hwa/v0/hwa.h:975
uint16_t srcShift
Definition: hwa/v0/hwa.h:836
int16_t dstAIdx
Definition: hwa/v0/hwa.h:898
HWA_PreProcessing preProcCfg
Definition: hwa/v0/hwa.h:1225
HWA Paramset Config.
Definition: hwa/v0/hwa.h:1204
uint32_t paramsetDone2
HWA interrupt priority for paramset done interrupt 2.
Definition: hwa/v0/hwa.h:1306
uint16_t srcAcnt
Definition: hwa/v0/hwa.h:823
uint32_t i_cmult_scale
Definition: hwa/v0/hwa.h:796
int32_t HWA_readDCEstimateReg(HWA_Handle handle, cmplx32ImRe_t *pbuf, uint8_t startIdx, uint8_t size)
Function to read the DC_EST_I/Q register.
HWA Paramset Config for Compression/Decompression block.
Definition: hwa/v0/hwa.h:999
uint8_t outputMode
Definition: hwa/v0/hwa.h:1180
void * callbackArg
Definition: hwa/v0/hwa.h:1243
HWA_SourceConfig source
Definition: hwa/v0/hwa.h:1215
#define HWA_NUM_RAMS
The number of RAM types in HWA.
Definition: hwa/v0/hwa.h:185
uint8_t ditherEnable
Definition: hwa/v0/hwa.h:1009
HWA_DoneInterruptCtx interruptCtxDone
interrupt context for all paramset done interrupt
Definition: hwa/v0/hwa.h:1426
bool bIsEnabled
Definition: hwa/v0/hwa.h:1359
uint8_t dstScale
Definition: hwa/v0/hwa.h:925
HWA Interrupt context structure for paramset done interrupt.
Definition: hwa/v0/hwa.h:1345
uint8_t twidFactorPattern
Definition: hwa/v0/hwa.h:1057
uint8_t dstRealComplex
Definition: hwa/v0/hwa.h:905
int32_t HWA_setSoftwareTrigger(HWA_Handle handle)
Function to manually trigger the execution of the state machine via software, the software trigger th...
uint32_t intNumParamSet
Definition: hwa/v0/hwa.h:595
HWA_Attrs const * hwAttrs
HWA Hardware related params.
Definition: hwa/v0/hwa.h:1390
uint8_t scaleFactorBW
Definition: hwa/v0/hwa.h:1021
uint16_t bCnt
Definition: hwa/v0/hwa.h:632
HWA_ComplexMultiply complexMultiply
Definition: hwa/v0/hwa.h:1223
HWA RAM Parameters.
Definition: hwa/v0/hwa.h:612
int32_t HWA_readDebugReg(HWA_Handle handle, HWA_DebugStats *pStats)
Function to read the debug registers (paramcurr, loopcou, acc_trig_in_stat)
uint16_t scale
Definition: hwa/v0/hwa.h:686
uint32_t instanceNum
Definition: hwa/v0/hwa.h:589
HWA Paramset Config for Output Formatter/Destination block.
Definition: hwa/v0/hwa.h:888
bool isCompressionEnginePresent
Definition: hwa/v0/hwa.h:602
int32_t HWA_readInterfChirpCountReg(HWA_Handle handle, uint16_t *numInterfSamplesChirp)
Function to read the number of samples that exceeded the threshold in a chirp.
void * HWA_Handle
A handle that is returned from a HWA_open() call.
Definition: hwa/v0/hwa.h:564
uint32_t instanceNum
HWA instance number.
Definition: hwa/v0/hwa.h:1371
HWA_Done_IntHandlerFuncPTR callbackFn
Definition: hwa/v0/hwa.h:1360
uint16_t numBanks
Definition: hwa/v0/hwa.h:1294
uint16_t srcAddr
Definition: hwa/v0/hwa.h:818
HWA Statistics from the STATISTICS block.
Definition: hwa/v0/hwa.h:1257
int32_t HWA_setSourceAddress(HWA_Handle handle, uint16_t paramIdx, uint32_t sourceAddress)
Function to set the source address for one paramset.
void HWA_deinit(void)
Function to deinitialize the HWA module.
int16_t srcAIdx
Definition: hwa/v0/hwa.h:827
int32_t HWA_readStatsReg(HWA_Handle handle, HWA_Stats *pStats, uint8_t numIter)
Function to read the 4 sets of 'MAX' statistics register.
uint32_t lfsrSeed
Definition: hwa/v0/hwa.h:679
int16_t dstBIdx
Definition: hwa/v0/hwa.h:901
uint16_t dstAcnt
Definition: hwa/v0/hwa.h:894
uint32_t maxValue
Definition: hwa/v0/hwa.h:1258
uint8_t bpmPhase
Definition: hwa/v0/hwa.h:877
uint8_t fftSize
Definition: hwa/v0/hwa.h:949
uint8_t accelMode
Definition: hwa/v0/hwa.h:1211
uint32_t qSumLSB
Definition: hwa/v0/hwa.h:1263
uint8_t windowEn
Definition: hwa/v0/hwa.h:964
HWA driver internal Config.
Definition: hwa/v0/hwa.h:1367
uint16_t currentLoopCount
Definition: hwa/v0/hwa.h:1278
HWA H/W Parameters.
Definition: hwa/v0/hwa.h:588
int32_t HWA_readIntfAccReg(HWA_Handle handle, uint64_t *accBuf, uint8_t type, uint8_t startIdx, uint8_t size)
Function to read the interference threshold MAG or MAGDIFF Accumulator register.
HWA_Object * gHwaObjectPtr[]
Externally defined driver object pointer.
uint8_t srcCircShiftWrap
Definition: hwa/v0/hwa.h:840