HWA Paramset Config for pre-processing block.
HWA paramset config parameters for the preprocessing block inside HWA_ParamConfig which is used with the HWA_ConfigParamSet() call.
Data Fields | |
uint8_t | dcEstResetMode |
uint8_t | dcSubEnable |
uint8_t | dcSubSelect |
uint8_t HWA_PreProcessing::dcEstResetMode |
controls the reset behavior for all 12 accumulators, see HWA_DCEST_INTERFSUM_RESET_MODE macros for correct values. set into HWA_DCEST_INTERFSUM_RESET_MODE_NOUPDATE to bybass DC estimation. sets the bits DCEST_RESET_MODE in register PREPROC in paramset
uint8_t HWA_PreProcessing::dcSubEnable |
enable/bypass DC subtraction, see HWA_FEATURE_BIT macros for correct values. set into HWA_FEATURE_BIT_DISABLE to disable the DC subtraction. sets the bits DCSUB_EN of the register PREPROC in paramset
uint8_t HWA_PreProcessing::dcSubSelect |
see HWA_DCSUB_SELECT macros for the correct values sets bits DCSUB_SELECT of the register PREPROC in paramset